- Mon Dec 20, 2010 5:08 pm
#115876
Hi,
I bought the ACS712 Low Current Sensor Breakout - SEN-08883, but when I tried to use the sensor is not functioning as it should. I connected the sensor to a Arduino board and the sensor readings are always the same regardless of whether the sensor is connected to a circuit or not. I also tried to calibrate the sensor by following the procedure that is on the product page but without success. The information that exists on the Internet is minimal. Is there a manual or more information so I can see to put the sensor to work?
Thanks in advance,
Henrique Dias
I bought the ACS712 Low Current Sensor Breakout - SEN-08883, but when I tried to use the sensor is not functioning as it should. I connected the sensor to a Arduino board and the sensor readings are always the same regardless of whether the sensor is connected to a circuit or not. I also tried to calibrate the sensor by following the procedure that is on the product page but without success. The information that exists on the Internet is minimal. Is there a manual or more information so I can see to put the sensor to work?
Thanks in advance,
Henrique Dias