- Mon Oct 11, 2010 3:04 pm
#111198
I've been working on developing a power management circuit for my data logger project using a Single Cell Lithium-Ion Battery, a MCP73833 Li-Ion Charge Chip, and a DC-DC converter to regulate the power supply. I would like to create a regulated 3.3V using the battery as the voltage supply, but I've been having a hard time finding a buck/boost IC to do the job. My design criteria are: 1) an IC that can be prototyped (no no-lead packages), 2) regulated 3.3V output, and 3) at least 100mA of current output. Does anyone have any suggestions for a buck/boost chip that fits these criteria?
I have tried the MCP1253-33X50 (http://ww1.microchip.com/downloads/en/D ... 21752a.pdf), but I have not had success in getting the power specified in the datasheet. I mounted the chip on an etched circuit board, used capacitors specified, and tested the circuit provided in the datasheet (pg. 12 - Select to Vin for 3.3V). I am only getting 20mA instead of the expected 100-120mA. When I check the output with a scope, there is very little noise (~5-10mV) for the 3.3V response. If someone is familiar with this chip, I'd appreciate suggestions for trouble-shooting this problem.
Thank you for your time and input.
-Crystal
I have tried the MCP1253-33X50 (http://ww1.microchip.com/downloads/en/D ... 21752a.pdf), but I have not had success in getting the power specified in the datasheet. I mounted the chip on an etched circuit board, used capacitors specified, and tested the circuit provided in the datasheet (pg. 12 - Select to Vin for 3.3V). I am only getting 20mA instead of the expected 100-120mA. When I check the output with a scope, there is very little noise (~5-10mV) for the 3.3V response. If someone is familiar with this chip, I'd appreciate suggestions for trouble-shooting this problem.
Thank you for your time and input.
-Crystal