- Sat Oct 02, 2010 1:20 pm
#110644
I'm not entirely sure if this is the proper forum for this question, but thought someone here might be able to help. I have a rainwater collection system that I am using to fill our toilet. Right now I have PEX tubing coming from both our utility water and the rain barrels. These lines each have a ball valve on them before intersecting at a T. The other side of the T goes to the toilet. This setup allows me to switch both ball valves and make use of either water source (handy during dry times of the year when we drain the barrels). By opening them both I can also fill the rain barrels which has come in handy while debugging this system and checking for leaks and whatnot. The unsavory part of this setup is that I have to crawl underneath my house in order to make the switch. I would love to be able to press a button in the house and have the ball valves electronically toggled for me. It seems like an Arduino could be used to control this pretty easily. Eventually it would be cool to have a water level switch of some kind on the rain barrels so that when they get low enough the Arduino would just switch the ball valves to the utility water without me even having to think about it.
Has anyone done anything like this before and know of a good source for electronically controlled ball valves? I do have easy access to utility power (110v) underneath the house so there wouldn't be any need for a battery powered solution. The lines in question are 1/2" PEX tubing.
Thanks for any help you can provide.
Has anyone done anything like this before and know of a good source for electronically controlled ball valves? I do have easy access to utility power (110v) underneath the house so there wouldn't be any need for a battery powered solution. The lines in question are 1/2" PEX tubing.
Thanks for any help you can provide.