- Sat Jun 12, 2010 12:13 pm
#102914
Well I've followed the first few beginning embeded electronics tutorials on the ATMega168 without any problems. I recently decided to mess around with UART, so I followed tutorial 4 to get my max232 working, then moved on to tutorial 5. But thats where I am having problems. I've double checked my wiring against the schematic and it's all correct. All I did from tut 4 to tut 5 was hook the rx/tx lines from my atmega168 to the rx/tx lines of the max232 like the tutorial says to. But no matter what I do I don't get any output in hyperterminal. I've double checked the rx/tx lines with a meter, and noticed that when my atmega168 outputs a message using the tutorials source code, the tx line will spike high, but the rx line is always low no matter what. Could this be the problem?