- Fri May 07, 2010 2:52 pm
#100382
I'm going to be making an external iPod battery using the 2000mAh Lithium Ion battery cell. The Lithium battery out outputs 3.7v The iPod charges at 5V 500-1000mA. Of course I'm shooting for 1 Amp if I can, it will take up an hour tops to re-charge/run the iPod. The 5V step-up I found at Sparkfun can only handle 300mA?
Is there any way to modify this step-up with higher rated parts that can handle 1 ampre? or even 500mA?
Is there any way to modify this step-up with higher rated parts that can handle 1 ampre? or even 500mA?