COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Have questions about a SparkFun product or board? This is the place to be.

Moderator: phalanx

Post Reply
noptical
Posts: 103
Joined: Mon Mar 03, 2008 3:18 pm

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by noptical » Sun Mar 28, 2010 7:04 am

this is great, why dont you post some more info :)

angelsix
Posts: 470
Joined: Thu May 07, 2009 4:10 am

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by angelsix » Sun Mar 28, 2010 8:03 am

Well I don't know about anyone else but I am just getting tired of this guy posting saying he has hacked LCDs. Big deal, why does anyone else care and why does he seem so needy to mention "I am 100% sure I am the first". Controlling LCDs are mostly all identical, and with a scope and enough time any LCD can be programmed without the datasheet. The reason no one is doing this is because what is the point. Why waste time and money figuring out the interface for an unknown screen instead of just buying a known one with a datasheet? Perhaps the challenge and pleasure of managing it for a screen or 2, but why sit there and just take apart countless phone screens and program them, if its been done once its been done a million times.

What would be more constructive and interesting to people is to actually make a post about what you do, your general procedures for figuring out the interface standards and the likes, and document things like that. At least they are beneficial and partially interesting.

mikeselectricstuff
Posts: 72
Joined: Sat Sep 06, 2008 12:34 pm

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by mikeselectricstuff » Tue Mar 30, 2010 4:01 pm

Why waste time and money figuring out the interface for an unknown screen instead of just buying a known one with a datasheet?
Because the 'unknown' ones used in high-volume consumer electronics are often available a lot cheaper and easier to get hold of as spares than ones that come with datasheets.
However issues like connector non-availability , like the ipod one and not-quite-compatible clone controllers (like some batches of the Sparkfun 6610 ones) can spoil the party.

However it really isn't a big deal to reverse-engineer LCD protocols if you have the device that the LCD came from - although some people seem to get rather over-excited about it. The trickiest bit is usually breaking out the fine-pitch connector while keeping the product in a sufficiently working state.

TheDirty
Support Volunteer
Posts: 657
Joined: Sun Jan 04, 2009 8:06 am
Location: Toronto, ON, Canada

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by TheDirty » Wed Mar 31, 2010 6:56 am

Looks good. LCD isn't too expensive, either.

Waiting on the tutorial, thanks.
Mark Higgins

angelsix
Posts: 470
Joined: Thu May 07, 2009 4:10 am

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by angelsix » Thu Apr 01, 2010 5:30 am

I figured the cheapness was a nice option, I liked programming the £3 Nokia black and white screen. However, from any form of non-commercial use (or mass use)surely they aren't really bothered about saving £5 and wasting hours hacking it. From a commercial front or mass use you would save a lot more, however if it was mass use, I would then still not use it as I would prefer a guaranteed supply and function.

For example I get full colour TFT's 3.5" with touchscreen, FFC cable and the works for £15 per unit in low volume. Find that anywhere else on a knock off screen for any noticeable difference and I will be impressed.

Luke

TheDirty
Support Volunteer
Posts: 657
Joined: Sun Jan 04, 2009 8:06 am
Location: Toronto, ON, Canada

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by TheDirty » Thu Apr 01, 2010 4:04 pm

I'm not understanding your problem with this. These screens on eBay look like they are going for about $8 each shipped for singles. For a hobbyist, that's a good deal if it's not that difficult to control. Your 3.5" solution is 3 times the price. You have lots of money if you are not bothered with saving £5 and I'm pretty sure you are in the minority.

The Nokia 128x128 goes for $15 here and I'm sure they sell tons of them.
Mark Higgins


TheDirty
Support Volunteer
Posts: 657
Joined: Sun Jan 04, 2009 8:06 am
Location: Toronto, ON, Canada

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by TheDirty » Fri Apr 02, 2010 1:35 pm

Thanks.

Translation: http://translate.google.com/translate?j ... l=pl&tl=en
Datasheet: http://www.trulydisplays.com/tft/driver ... LDS285.pdf

Well, according to the guide the IO voltage cannot go over 1.95V (guide says 1.8V, spec says 1.95V). You could change this if you could get access to the PSEL pin on the controller, but I guess you can't.

The PSEL (power level selection) pin maybe one of the ones he just tied to ground. If that limitation can't be gotten around it makes this LCD not very attractive for me.
Mark Higgins

WGR7
Posts: 1
Joined: Thu Sep 09, 2010 7:05 am

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by WGR7 » Thu Sep 09, 2010 7:10 am

Hi Maan2k,

I've seen the page:
http://www.elektroda.pl/rtvforum/viewto ... 2263350eea

I have a questions.

What is the value of the LED resistor and the voltage for this resistor?

gonzodada
Posts: 33
Joined: Mon Jul 19, 2010 3:22 pm

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by gonzodada » Fri Sep 10, 2010 2:37 am

You're being a tiny bit grumpy but I do understand why you find it annoying :) There's a guy on a forum I frequent that gives an answer to like every single post even if he doesn't really know the answer, which is nearly always! I just can't help thinking, "Oh God. You again! Do shut up."

MrZANE
Posts: 1
Joined: Tue Nov 09, 2010 7:35 am

Re: COLOR NOKIA E51 LCD IS FINALLY HACKED 240x320 Pixels

Post by MrZANE » Fri Nov 12, 2010 4:38 am

Hi everyone.

Is there anybody that knows the manufacturer and article# of the SMD PCB receptacle for the E51/6700c LCD?

TIA
/Jimmy

Post Reply