- Wed Feb 24, 2010 3:15 pm
#94449
@ tetsujin,
Well, perhaps I should restrict myself to posting educated guesses. ;o} Thanks for the correction!
@lordsteve,
What are you calling "left side" and "right side"? Specifically, are you referring to the right and left audio channels or the right and left sides of the jack assembly?
It would be helpful to us if you told us what you have connected to where and which pins (by name/number) have continuity to each other with the jack empty and with the jack filled by a stereo plug. Also, when you do the test, you need to have the stereo plug not wired to anything. If the plug is wired to anything, that "anything" may well change the results.
For example, if you have nothing connected to the jack and nothing connected to the plug, then the Ground, Ring, and Tip connections of the jack should be shorted to the sleeve, ring, and tip of the plug, respectively. However, the Ground/sleeve, ring, and tip should be isolated from each other.
Conversely, if you have the plug wired to a set of speakers/headphones with each side of the speakers having an resistance of R ohms, then the resistances, measured from the jack connections, should be:
Ground <> Ring: R + r
Ground <> Tip: R + r
Ring <> Tip: 2R + r
(r is the resistance of the jack's internal connections to itself and the plug. It may be too small for you to measure.)
My understanding of the "shunt" connections is that they are connected to the corresponding signal inputs when there is no plug in the jack and disconnected when a plug is inserted. That behavior allows using them to connect a speaker that is muted by the insertion of a plug.
Please let us know what, if anything, you had wired to the plug when you did your testing and how much resistance you had that you are calling "shorted". Also, if there is something wired to the plug, what are the resistances between the pairs of contact areas on the plug?
TIA,
Eric