- Fri Nov 13, 2009 6:14 pm
#85051
It like to drive my graphic serial backpack and 128x160 LCD off a 5V supply used for the rest of my project. As it is, the backpack is supposed to be driven at 6V-7V which is awkward and, for me, very impractical, but that is simply so the regulator on the backpack can deliver 5V. At 5V regulator on the backpack drops the voltage too low for the LCD text to be readable, but the LCD itself is supposed to run well at 5V.
Can the regulator on the backpack be short circuited (jumpered) so that the unregulated 5V runs both the backpack and the LCD? If my supply voltage is clean it looks from the schematic that this should work. If I run it off a USB-serial, then I am guessing I will get a clean enough 5V not to require the regulation. Any thoughts or suggestions?
Can the regulator on the backpack be short circuited (jumpered) so that the unregulated 5V runs both the backpack and the LCD? If my supply voltage is clean it looks from the schematic that this should work. If I run it off a USB-serial, then I am guessing I will get a clean enough 5V not to require the regulation. Any thoughts or suggestions?