- Fri Oct 21, 2005 10:50 pm
#7421
Hey all,
I got 8 power supplies from Sparkfun, and I'm a bit confused... well, very confused
On the website, it says two 100uF capacitors in the parts list. In the schematic, it also says two 100uF capacitors (C1 and C2). However, in the photos, its easy to tell the capacitors are not the same, and looking at the PCB you can see that the circles are different sizes (larger for C1 than C2).
So, should there be two 100uF capacitors in the packages, or a 100uF for C1 and a 10uF for C2? I was shipped a 100uF and a 10uF in all 8 packages.
If it should be 10 and 100, does it matter which is which? Before I even realized that one wasn't a 100uF capacitor, I soldered it into C1, and now can't get it out for the life of me
Thanks!
Grecko
PS> I'm switching the voltage regulator included for a 2.5v 5A regulator, if it affects the needed capacitors at all.
I got 8 power supplies from Sparkfun, and I'm a bit confused... well, very confused
On the website, it says two 100uF capacitors in the parts list. In the schematic, it also says two 100uF capacitors (C1 and C2). However, in the photos, its easy to tell the capacitors are not the same, and looking at the PCB you can see that the circles are different sizes (larger for C1 than C2).
So, should there be two 100uF capacitors in the packages, or a 100uF for C1 and a 10uF for C2? I was shipped a 100uF and a 10uF in all 8 packages.
If it should be 10 and 100, does it matter which is which? Before I even realized that one wasn't a 100uF capacitor, I soldered it into C1, and now can't get it out for the life of me
Thanks!
Grecko
PS> I'm switching the voltage regulator included for a 2.5v 5A regulator, if it affects the needed capacitors at all.