- Wed Oct 28, 2009 12:15 pm
#83876
Hello, I recently purchased a Serial Enabled 16x2 LCD - White on Black 5V
sku: LCD-09395
and got it working with my Arduino relatively quickly. Had a few problems with the text wrapping, but that is a separate issue.
(1) PROBLEM: when the Arduino gets its power from my Mac via USB, the LCD displays the splash screen and then writes the text from my arduino script just fine.
BUT: when i connect the arduino to a verified 5v external power supply, the LCD turns "on" but the characters that it displays are incredibly dim, at fist i though that it was not working, but will all other light off, i can barely make out that the LCD is still working.
Any ideas what i have to adjust? It should be getting 5v, because it is connected to the 5v pin of the arduino, and the arduino is getting 5v from the power adapter.
thanks for any suggestions!
(2) The other issue is that if i feed the LCD a serial.print("some text") command and the "some text" string is longer than one line on the LCD, it drops a character or two when it auto-wraps to line two.
-Octagon26
sku: LCD-09395
and got it working with my Arduino relatively quickly. Had a few problems with the text wrapping, but that is a separate issue.
(1) PROBLEM: when the Arduino gets its power from my Mac via USB, the LCD displays the splash screen and then writes the text from my arduino script just fine.
BUT: when i connect the arduino to a verified 5v external power supply, the LCD turns "on" but the characters that it displays are incredibly dim, at fist i though that it was not working, but will all other light off, i can barely make out that the LCD is still working.
Any ideas what i have to adjust? It should be getting 5v, because it is connected to the 5v pin of the arduino, and the arduino is getting 5v from the power adapter.
thanks for any suggestions!
(2) The other issue is that if i feed the LCD a serial.print("some text") command and the "some text" string is longer than one line on the LCD, it drops a character or two when it auto-wraps to line two.
-Octagon26