- Sat Oct 03, 2009 9:33 am
#82258
I am having a problem with my text file that is generated. I expect the header and I can set Matlab/Octave to ignore that. What is more difficult to deal with are periodic data inserts of this nature:
If anyone that can point me as to what is needed to happen to make this show up in a data log with my initialization file, I'd appreciate it. As you can see, I am using text and logging battery voltage and 2 analog channels.
Code: Select all
How is the PPS triggered? I would not mind having this in the header as it has the time in it, but having this show up periodically in the data set is a bit problematic. Also, that it drops off one of the logged channels is also a bit of a problem, but not a huge biggie. 637 6300 380 2190
637 6300 380 2192
PPS: 20090930,132422.937397
$PKWNP,20090930,132422.937397*79
309 4819 2549
637 6309 4756 2526
637 6308 4521 2516
If anyone that can point me as to what is needed to happen to make this show up in a data log with my initialization file, I'd appreciate it. As you can see, I am using text and logging battery voltage and 2 analog channels.
Code: Select all
KeithGUART0 mode=None
UART0 baud=0
UART0 trigger=$
UART0 end=0x0A
UART0 size=64
UART0 timestamp=N
UART1 mode=None
UART1 baud=0
UART1 trigger=$
UART1 end=0x0A
UART1 size=64
UART1 timestamp=N
Start Time=20090922084500
Powersave=1
ADC mode=Text
ADC frequency=10
ADC binning=10
AD0=Y
AD1=Y
AD2=Y
AD3=N
AD4=N
AD5=N
AD6=N
AD7=N
AD8=N