- Mon Jun 15, 2009 8:05 am
#74989
The piezo idea is possibly the easiest to implement. Simply attached any type of piezo electric material to moving parts can gather energy. However, always remember basic thermodynamics. By adding piezo components to moving parts will add extra load and resistance to the machine (human, etc.)
It may be advantageous to try to gather truly wasted energy, such as heat (which if not tapped would simply leave the system)... Muscles heat up when you walk and adding thermoelectric converters around them would generate electricity as well as help cool you down (since they would conduct the heat away, possibly better than sweat evaporation).... Current, efficient thermoelectric converters are lacking efficiency.
Another method to more directly steal the kinetic energy is by use of lasers and blue shifting. Shine a laser toward something in relative negative motion with your body ( I mean that something always approaching you, like the ground before you. If you choose the right angles, use photomultipliers, and very high efficiency optics you can actually trade in some of your body's momentum for a very low current, high voltage energy. Hmm... it would probably require technology to advanced currently. But essentially you could get very high yields back from it.
And finally, best for last!!! Use gyroscopes. As you move and change orientations, the highspeed gyroscope will rotate relative to you and if geared properly, it can directly spin a generator. I don't mean using the gyroscope's flywheel, i mean use the gyroscope's entire body to rotate a gear box to spin the generator. The gyroscope as a whole will only rotate around it's axis when you move. For this to work you will need zero friction bearings (they do exist), but it may still be an engineering challenge. Physically, it's pretty simple though, and simply converts your momentum to electricity. With a high wattage version of this system, your body WILL notice an increased difficulty in moving. Try taking a toy gyroscope spinning at 100,000 RPM... it's much harder to accelerate it!
Jesse Randall
Electronic Engineer
Design Coordinator
http://www.NovaConceptions.com