- Sun Mar 29, 2009 4:31 pm
#69566
I'm at the tail end of a project i've been working on for a while now. Hooray!
In my device, i'm using a LM7805 voltage regulator (http://www.sparkfun.com/commerce/produc ... cts_id=107) to bring the 9v wall wart adapter down to a regulated 5v for my project. The 7805 is generating a bit of heat trying to dissipate that extra 4v (actually, i'm not sure if this is how it works... i'm pretty new to electronics). I've attached a heat sink (http://www.radioshack.com/product/index ... Id=2102857) to it and it's still a bit warm.
The device is enclosed in a wooden case, which has a fair amount of breathing room & an open back. The warmth being generated probably isn't that hot. I can touch the bottom side of the regulator with my finger. The heat sink is noticeably warm, but not too much above room temperature. I used hooked up a digital thermometer (http://www.sparkfun.com/commerce/produc ... cts_id=245) and and arduino to the hottest part and it seems to top out around 90 degrees F after a few hours.
The device is something that is running all the time. Is there anything i need to worry about? If for some reason it gets hot enough to do some damage, would the regulator stop working before a fire broke out?
I appreciate your input.
In my device, i'm using a LM7805 voltage regulator (http://www.sparkfun.com/commerce/produc ... cts_id=107) to bring the 9v wall wart adapter down to a regulated 5v for my project. The 7805 is generating a bit of heat trying to dissipate that extra 4v (actually, i'm not sure if this is how it works... i'm pretty new to electronics). I've attached a heat sink (http://www.radioshack.com/product/index ... Id=2102857) to it and it's still a bit warm.
The device is enclosed in a wooden case, which has a fair amount of breathing room & an open back. The warmth being generated probably isn't that hot. I can touch the bottom side of the regulator with my finger. The heat sink is noticeably warm, but not too much above room temperature. I used hooked up a digital thermometer (http://www.sparkfun.com/commerce/produc ... cts_id=245) and and arduino to the hottest part and it seems to top out around 90 degrees F after a few hours.
The device is something that is running all the time. Is there anything i need to worry about? If for some reason it gets hot enough to do some damage, would the regulator stop working before a fire broke out?
I appreciate your input.