noptical wrote:Here's something I thought, someone with more experience please correct me if that wont work.
Apply solder paste on the holes/pads on solder side of the pcb. Place all the leds through the holes, there will be enough solder paste around the leads. Flip the board (place something over the leads so they dont come out when you flip it) and use a hot air gun to heat the pads where the paste is. Trim the leads.
Excellent Idea! Hopefully someone will try this and report
back here.
The problem is going to be displacement of the solder
paste when the leaded parts are inserted into the holes.
Another issue is the paste may cause bridges (shorts) if
capillary action doesn't pull it to the pads. Watching SMT
soldering by IR or hot air shows the molten solder is
pulled onto the pads as it liquifies.
There is a company that makes "solder washers" which
can be placed over a leaded part and then melted down.
It would be tedious to do this for all leads one at a time,
but the mass soldering by IR or hot air would pay off.
There is a strong case here to redesign in SMD/SMT only.