OK, so making a solenoid seems a great idea as it turn out. I can make two, with inverse polarity that pull/push the blade actuator lever, on each sides...
So to make a solenoid, I have (isolated) copper wire, and I just need to wind a large amount around a non-conductive core (small plastic tube) where I can slide the metal rod ? How much is 'much' here ? 1 meter ? would thinner wire work better than thicker wire ?
Also, on how to actuate the solenoid; I will have to use some isolation so I was thinking 'mosfet' -- however by looking a bit deeper there seems to be "mosfet drivers" ICs that output short, low current, high voltage and it seems it's just what I want... so I've been wondering if I could use /that/, directly to power the solenoid itself... does that make sense ? Remember I'm a newb; a creative newb (the dangerous kind
)
I've read that I need to have good isolation, including reverse current; I wonder if these mosfet drivers have that, and what sort of specs I'd need if I needed a clamping diode..
Thanks for the input so far!