- Mon May 12, 2008 2:09 pm
#48129
I recently purchased a dozen of the TCM8230MD 640x480 camera modules. Using my circuit plotter I created a small surface mount board and soldered the module along with the 2.8V and 1.5V SOT-23 regulators along with outputs for each of the pins. The surface mount components were assembled using solder paste. I designed an EAGLE part for the camera. I have my Tektronix TDS2024B Oscilloscope connected to my prototyping board that has the 0.1" pitch header coming from the camera interfacing with my Atmel AT91SAM7S64 ARM development board. I am generating a 15MHz clock signal for the camera, reset is high (off), the regulators are outputing the correct voltage, and I have the I2C (TWI) lines pulled high with a 1k resistor. As of right now it looks like the I2C clock line is not sinking when interfaced with the module and I detect no shorts. After digging around it turns out this camera originally came with a socket to be used for the soldering process so that the camera does not get damaged. Has anyone had any success in communicating with this camera yet?