- Thu Apr 03, 2008 7:34 pm
#45808
saipan59 wrote:That's interesting. How long is that timer running? So when the PIC sends data the low pulse will trigger the 555. I wonder if 5V from the PIC would be enough to keep the 555 from triggering with a 12V VCC. Do you find that the xmtr powers up fast enough or do you lose a byte or two before it powers up? I'm sure I have a 555 around here I could test that with.
FYI, a possible variation on my circuit:
Change the CMOS 555 to the traditional bipolar type (which has much greater drive capability), and let the output of the 555 provide power to the xmtr module *directly*, eliminating both transistors. You get the benefit of the "automatic xmtr power-on/off", you don't need to use an extra PIC pin, and the overall circuit is rather simple.
Pete