Logic Level Converter - Single Supply Voltage In

Have questions about a SparkFun product or board? This is the place to be.

Moderator: phalanx

Post Reply
erdc
Posts: 7
Joined: Mon Jan 18, 2016 3:11 pm

Logic Level Converter - Single Supply Voltage In

Post by erdc » Wed Aug 15, 2018 8:38 am

In the description of this part (PRT-14765) it states:
"What makes this Logic level converter truly special is the fact that you can supply it with 3.3V and it will create the 5V"
But the stencil on the PCB shows that you can give it 3-5.5V, and that suggest that as long as you are within this voltage range, you will get both 3.3V and 5V of output. Is this a correct assumption?

darrellg
Posts: 359
Joined: Fri Oct 17, 2014 10:02 am
Location: Southern California

Re: Logic Level Converter - Single Supply Voltage In

Post by darrellg » Wed Aug 15, 2018 8:51 am


erdc
Posts: 7
Joined: Mon Jan 18, 2016 3:11 pm

Re: Logic Level Converter - Single Supply Voltage In

Post by erdc » Wed Aug 15, 2018 11:05 am

That link is where I got my quote from.

User avatar
DanV
Posts: 396
Joined: Sat Apr 25, 2015 9:29 am

Re: Logic Level Converter - Single Supply Voltage In

Post by DanV » Wed Aug 15, 2018 11:31 am

Have a look at this page where it clearly states you can supply 3.3 and get 5V out and it further refines it to 3.3V output as well.

https://learn.sparkfun.com/tutorials/si ... e-overview

therealclimber
Posts: 1
Joined: Wed Jan 23, 2019 4:38 pm

Re: Logic Level Converter - Single Supply Voltage In

Post by therealclimber » Wed Jan 23, 2019 4:48 pm

Hello there;

I just got one of these and when I hooked up 4.9 volts to VIN and GND on the upper left it immediately smoked. Nothing else was hooked up. I confirmed the polarity and voltage of the power both before and after. I need bi-directional level conversion and power is only available from the +5 side. I have another one but I'm afraid of trying it lest I smoke that one as well. I read the hookup guide and nothing indicated I had to do anything else to make it go. Am I missing something? Thanks!

darrellg
Posts: 359
Joined: Fri Oct 17, 2014 10:02 am
Location: Southern California

Re: Logic Level Converter - Single Supply Voltage In

Post by darrellg » Thu Jan 24, 2019 9:26 am

If you are certain it was connected correctly, then you should contact Sparkfun support (https://www.sparkfun.com/support) and ask them what your next step is.

Post Reply