Raspberry Pi 3 Model B V1.2, will not boot with Sparkfun power supply

Have questions about a SparkFun product or board? This is the place to be.

Moderator: phalanx

Post Reply
cappy
Posts: 14
Joined: Thu Sep 22, 2011 2:10 pm

Raspberry Pi 3 Model B V1.2, will not boot with Sparkfun power supply

Post by cappy » Wed Jul 11, 2018 5:49 pm

I've recently bought 2 of these power supplies, for my R Pi3s..
https://www.sparkfun.com/products/13831

It seems like the output voltage is too low for the Rpi,
as it does not boot. The red power LED comes on, the green LED blinks, the yellow ethernet link LED
comes on too, but nothing on the monitor.

Using a similar power supply that I had bought from Adafruit a while back,
https://www.adafruit.com/product/1995 (note, the actual voltage written on this power supply is 5.25V)
"Note: As of Tuesday, March 22nd 2016, we are now shipping an updated 5.25V 2.4A version of this power supply."

the same R Pi 3 has no problem booting.

Do the lower voltage power supplies work for you on your R Pi 3s?

thanks

BLH
Posts: 20
Joined: Tue May 29, 2018 4:50 am

Re: Raspberry Pi 3 Model B V1.2, will not boot with Sparkfun power supply

Post by BLH » Sat Jul 14, 2018 4:39 am

The official Raspberry Pi Organization power supply is 5.1 Volts 2.5 Amps.
I don't think that should not be a problem.
I know some sellers are using 5.25 Volt 2.5 amp supplies. I don't believe it is a requirement.
I got a kit from MCM and it came with a 5.25 Volt 2.4 Amp.
Is there anyway you could safely measure the 5 volts on the board. Maybe on the connector used for Hats or a deice poweed through one of the USB Ports?

Post Reply