- Sun Apr 15, 2018 12:01 pm
#198958
Hey guys, i'm hoping someone can help me decide the best relay to purchase from SF for controlling a 1/2hp inductive load 120v motor. I've spent numerous days researching this and hoping someone with more experience could help me clarify a few things.
Relay will be controlled by some type of microcontroller, probably an ESP32 or maybe even a Pi (not sure yet), but would be 3.3v or 5v GPIO to control the relay.
Application:
Hoping that someone with a little more experience in this than I have could provide any feedback based on past experiences or knowledge. Thanks ahead of time for your help, and for taking the time to read this
Relay will be controlled by some type of microcontroller, probably an ESP32 or maybe even a Pi (not sure yet), but would be 3.3v or 5v GPIO to control the relay.
Application:
- 110-120v 1/2 HP electric motor --- 7.2a at full load
- Runtime anywhere from 30-60 seconds, twice a day (up to 10 times a day, with ~30 second runtime)
- Installation will be inside sealed IP65 enclosure with DIN rail
- Microcontroller or Pi Zero W (undecided as of now) will be mounted on DIN rail
- SPST/SPDT Electromechanical Relay (SPST more than likely) - https://www.sparkfun.com/products/13815
- 40a Solid State Relay (i've found clips for DIN rail mounting for these) - https://www.sparkfun.com/products/13015
- Din Rail SPST Relay - TBD
- SPST Electromechanical Relay Lifespan - One concern of mine is the lifespan of an electromechanical relay, given the fact that my setup could essentially have up to 10 on/off cycles per day --- what kind of lifespan could I expect for an electromechanical relay in my type of setup with an inductive load from a motor?
- Inductive Load on Electromechanical Relay - One other concern I have is that the relay would be driving an inductive load from the motor ... do anybody have any experience, warnings, suggestions, or thoughts on this?
- Solid State Relay Heat - My concern regarding the solid state relay is the heat generated from it, as I have seen a lot of them that require a heatsink ... my question is, with my load only being a max of 7.2a and runtimes being very low (30-90 seconds max), is this something I would need to be concerned with? I ordered both relays to test with, and some temp strips to get max temp it gets to, but wondering if anybody has any insight or history regarding this?
- Price Points - The electromechanical relays tend to all be cheaper in price, but in my project is it worth the ~$5-10 savings as in regards to having an SSR which would have a longer lifespan than the EMR? If my prototype turns out to work well, I may eventually want to turn this into a commercial product, so price at that time would be a concern, but I also want to consider quality/lifespan of product based on having a lot of cycles on the relay.
- DIN Rail Mountable SPST Electromechanical Relays - As my project will be inside an enclosure with DIN rail, my first thought was to look at buying an SPST EM relay, but my concern with that is regarding the protection of the GPIO from the MC ... does anybody have experience using any of these, or what I should look to make sure is included in the relay to protect the MC (like snubber circuit)? I'm not sure if there's a specific term used for DIN rail relays that specifies it has some type of snubber circuit integrated in it.
Hoping that someone with a little more experience in this than I have could provide any feedback based on past experiences or knowledge. Thanks ahead of time for your help, and for taking the time to read this