- Mon Oct 08, 2007 7:00 am
#36069
Hello,
i've bought two samples of bluetooth DIP module WRL-08461. As far as i've read, the only difference with the previous module is that this one has an active low output for the Status pin. The problem is that, whether i connect or not, the status of this pin is always "low". The only change that i can see is on the pin number 5 on JP1 (wich should be PCM_CLK. two pins away from the RESET one, according to the sheet on http://www.sparkfun.com/datasheets/Wire ... ematic.pdf ), that ranges from 1.8V when not connected, to zero when there is a connection. The status pin of the previous module was number 5 on JP2 (close to the CTS one) and remain always zero. Any suggestion?
Uriel
i've bought two samples of bluetooth DIP module WRL-08461. As far as i've read, the only difference with the previous module is that this one has an active low output for the Status pin. The problem is that, whether i connect or not, the status of this pin is always "low". The only change that i can see is on the pin number 5 on JP1 (wich should be PCM_CLK. two pins away from the RESET one, according to the sheet on http://www.sparkfun.com/datasheets/Wire ... ematic.pdf ), that ranges from 1.8V when not connected, to zero when there is a connection. The status pin of the previous module was number 5 on JP2 (close to the CTS one) and remain always zero. Any suggestion?
Uriel