SparkFun Forums 

Where electronics enthusiasts find answers.

All things pertaining to wireless and RF links
By Draradech
#35452
Hello.

If I want to connect the BlueSMiRF to the EM-406A, do I need external parts?
Or does it suffice to provide power, short RTS/CTS on the BlueSMiRF and connect RX to TX and TX to RX?
(Is it really that simple?)

Thanks, Draradech
By daemondust
#35527
I've successfully connected them directly. Make sure you're running the BlueSMiRF at 3.3v. Actually, I was able to run both off of a regulated 3.3v line without any problems.

Remember that the baud rate for the EM-406 and BlueSMiRF are independent of each other, and have to be in sync.