- Wed Jun 27, 2007 12:40 pm
#31902
Ok, so here is my problem:
I have two components, a base station and a key. I want the base station to be able to excite a voltage on the key without the key having to use any power of its own. So, I am using the Friis Transmission Equation to compute the power on the receiving antenna and then converting that to a voltage. Here is my matlab file and the results,
Im using the nRF24L01 and the chip antennas on both sides.
Thanks,
Brandon
I have two components, a base station and a key. I want the base station to be able to excite a voltage on the key without the key having to use any power of its own. So, I am using the Friis Transmission Equation to compute the power on the receiving antenna and then converting that to a voltage. Here is my matlab file and the results,
Code: Select all
% General
freq = 125e3; % Hz
C = 299792458; % m/s
D = 2.0; % m
% Transmission Power
Pt = 1e-3; % W, = 0dBm
% Transmission Antenna
Gt = 1.2; % W, = 0.8dBi
Rt = 50; % Ohm
% Receiving Antenna
Gr = 1.2; % W, = 0.8dBi
Rr = 50; % Ohm
% Receiving Power
Pr = ( Pt * Gt * Gr * ( C / freq )^2 ) / ( 4 * pi() * D )^2
% Voltage In
sqrt( Pr * Rr )
Code: Select all
So, does that mean that 25V will be received? That cant be handled by a pic so some conditioning of the signal must be done, like stepping it down to 5V and then rectifying it?Pr = 13.1131
ans = 25.6057
Im using the nRF24L01 and the chip antennas on both sides.
Thanks,
Brandon