- Thu Jun 14, 2007 6:12 pm
#31354
Hello,
My name is Diego and I 'm from Cali, Colombia. I bought several Bluetooth Modem - BlueSMiRF from Spark Fun Electronics and I'm configuring the Bluetooth Modems using ATMP COMMANDS.
The problem is that I configured a Bluetooth Modem to be as Auto-Master (ATSW25,1,1,0,0) but I forgot to put the ATSMA command with the Slave Address and the UUID, when I try to access the Bluetooth Modem using the serial RX and TX I 'm not getting any answer, I try also to using the +++ command from the Blue Dongle.
Talking about power compsution when I turn on the Blueradio the Current is close to 40mA and after a few seconds (1 or 2) goes to almost 1mA or nothing.
the version is 3.5.2.1.3.0. I tried putting 3.3V on PIO4 on the start up of the Blueradio, but everything continues like it was.
I made the operation with other Bluetooth Modem as Master and I can get to comunicate to it using the serial RX and TX.
What do I need to do?.. Anyone with the Same Problem?..
Thank for your help, I will apreciate your answer
Diego Alejandro Gonzalez
University Javeriana
Cali
Colombia
My name is Diego and I 'm from Cali, Colombia. I bought several Bluetooth Modem - BlueSMiRF from Spark Fun Electronics and I'm configuring the Bluetooth Modems using ATMP COMMANDS.
The problem is that I configured a Bluetooth Modem to be as Auto-Master (ATSW25,1,1,0,0) but I forgot to put the ATSMA command with the Slave Address and the UUID, when I try to access the Bluetooth Modem using the serial RX and TX I 'm not getting any answer, I try also to using the +++ command from the Blue Dongle.
Talking about power compsution when I turn on the Blueradio the Current is close to 40mA and after a few seconds (1 or 2) goes to almost 1mA or nothing.
the version is 3.5.2.1.3.0. I tried putting 3.3V on PIO4 on the start up of the Blueradio, but everything continues like it was.
I made the operation with other Bluetooth Modem as Master and I can get to comunicate to it using the serial RX and TX.
What do I need to do?.. Anyone with the Same Problem?..
Thank for your help, I will apreciate your answer
Diego Alejandro Gonzalez
University Javeriana
Cali
Colombia