SparkFun Forums 

Where electronics enthusiasts find answers.

All things pertaining to wireless and RF links
By vane_caracas
#26237
Hi,

I have a doubt about the connection....

When I connect one hac-um96 to a pic i have to do it with the rs232 interface?? or this is direct (um96 to pic) and only use the rs232 to connect it to the PC.

Thanks.
By NleahciM
#26238
vane_caracas wrote:Hi,

I have a doubt about the connection....

When I connect one hac-um96 to a pic i have to do it with the rs232 interface?? or this is direct (um96 to pic) and only use the rs232 to connect it to the PC.

Thanks.
If you read the datasheet you'll see that the UM96 has both TTL and RS-232 level UARTs.

I would recommend using the TTL uart to connect directly to your PIC.
By n1ist
#26241
Use the TTL levels to connect directly to a 5V pic. Use the RS232 levels
to connect to a PC.