- Wed Jan 31, 2007 9:59 pm
#25781
Hello all, I have some questions on rf designs. I have a supply of receivers and transmitters here are the part numbers (KESRX01 290 - 460 MHz ASK Receiver ) and transmitter based on (RFM-RO2100 saw resonator). My questions are 1. Since both of these circuits use PIC microcontrollers can I remove the PIC's and use the receiver in my project with an AVR micro since I have the STK500 and some AVR's. I think I can do this with the receiver since I can just pick up from the data out pin without a problem. 2. I am not sure about the transmitter since it uses a resonator, so what can I do about that. Also since the frequency is set to 295MHZ how can I go with a different transmitter that will work with this receiver. I am trying not to build my own circuits since I have plenty of these, any idea's on how I can use these circuits would help. Thanks Lupe.