Hello All,
This is my first post and my first Arduino project. I am creating a Scoreboard with LEDs that I can control with a 4 button RF remote. The problem that I am having is that when a button on the remote is pressed it sends 4-5 signals to the receiver. So.. instead of the score going up by 1 it goes up by 4 or 5. I was hoping someone has some experience in this might be able to steer me in the right direction. Thank you in advance.
RF Remote to Receiver >Arduino for Scoreboard
Moderator: phalanx
Re: RF Remote to Receiver >Arduino for Scoreboard
normally each button on a remote has a unique code that can consist of multiple bytes. You can add a little code to read and check which unique code was received and update you scoreboard ( e.g. add 1 or 10, or subtract 1 or 10 etc).
Re: RF Remote to Receiver >Arduino for Scoreboard
How is the remote connected to the Arduino? If there is any kind of mechanical switching in your remote receiver (like a relay), you'll need to debounce the Arduino inputs.
Re: RF Remote to Receiver >Arduino for Scoreboard
Often rf remotes (or IR probably also) send multiple repeats of command packets. To ensure reception chances and verify for errors in transmission. Your arduino code would need to be smart enough to recognize and verify the repeats are the same. And once the command is received verified and understood implement a time delay to not execute the command (increase, decrease, reset) more than once within reasonable time.
As often (always), if you give more insight to what code it running on your Arduino then we might be able to provide more explicit suggestions.
As often (always), if you give more insight to what code it running on your Arduino then we might be able to provide more explicit suggestions.