Unviersal Reader Assistant

All things pertaining to wireless and RF links

Moderator: phalanx

Post Reply
marensofier
Posts: 1
Joined: Thu Jun 21, 2018 12:33 pm

Unviersal Reader Assistant

Post by marensofier » Wed Jun 27, 2018 5:06 am

I am using the M6e Nano rfid-reader module. It is connected only to USB and the settings given in the tutorial is used. I am using the Alien Higgs-3 UHF RFID Tags. When I try to read the user memory, inspect tags or any other operation than reading I get the error; "Specified port does not exist". It also says that the COM-port is not accessable. Are there any possible solutions or answers to this?

paulvha
Posts: 289
Joined: Sat Nov 11, 2017 2:39 am

Re: Unviersal Reader Assistant

Post by paulvha » Wed Jun 27, 2018 1:09 pm

make sure to connect to the M6E nano to USB before starting the URA (or use refresh).It will enable the right USB port to select. BEFORE reading, set the read power/write power to 500mW (max!) if powered by USB only before starting reading (you can connect)

Post Reply