SparkFun Forums 

Where electronics enthusiasts find answers.

All things pertaining to wireless and RF links
By marensofier
#199577
I am using the M6e Nano rfid-reader module. It is connected only to USB and the settings given in the tutorial is used. I am using the Alien Higgs-3 UHF RFID Tags. When I try to read the user memory, inspect tags or any other operation than reading I get the error; "Specified port does not exist". It also says that the COM-port is not accessable. Are there any possible solutions or answers to this?
By paulvha
#199587
make sure to connect to the M6E nano to USB before starting the URA (or use refresh).It will enable the right USB port to select. BEFORE reading, set the read power/write power to 500mW (max!) if powered by USB only before starting reading (you can connect)