How to transfer power wirelessly by Infrared

All things pertaining to wireless and RF links

Moderator: phalanx

Post Reply
rupamc6
Posts: 2
Joined: Fri Jun 09, 2017 3:16 am

How to transfer power wirelessly by Infrared

Post by rupamc6 » Fri Jun 09, 2017 3:18 am

Hello everyone, I wish to transfer power at a distance of 10-15 feet using Infrared diode/LED. I need 3-4V at receiver side. I have used normal IR diode of AC remote control, modulated by 38 to 100 kHz as a transmitter and photo-diode as a receiver. I have already tried to transfer the power, but unable to do the same. Please suggest me about the required components and circuit for transferring the above mentioned power.
Can any one help me?

User avatar
DanV
Posts: 333
Joined: Sat Apr 25, 2015 9:29 am

Re: How to transfer power wirelessly by Infrared

Post by DanV » Fri Jun 09, 2017 7:43 am

10 - 15 feet is a HUGE distance for this attempt.
Light intensity decreases inversely proportional to the square of the distance.
Increasing your distance by 2 times decreases the light intensity by 4 times.
Your chances of doing this are extremely slim.
Maybe a very large array of IR leds and a solar panel could provide something on the receiving end.

jremington
Support Volunteer
Posts: 2148
Joined: Fri Jun 15, 2007 9:41 pm
Location: Eugene, Or

Re: How to transfer power wirelessly by Infrared

Post by jremington » Fri Jun 09, 2017 1:59 pm

I need 3-4V at receiver side.
Voltage is not power.

Tell us what you actually want to do.

rupamc6
Posts: 2
Joined: Fri Jun 09, 2017 3:16 am

Re: How to transfer power wirelessly by Infrared

Post by rupamc6 » Fri Jun 09, 2017 10:08 pm

DanV wrote:10 - 15 feet is a HUGE distance for this attempt.
Light intensity decreases inversely proportional to the square of the distance.
Increasing your distance by 2 times decreases the light intensity by 4 times.
Your chances of doing this are extremely slim.
Maybe a very large array of IR leds and a solar panel could provide something on the receiving end.
I have supplied power to IR LED from function generator.
Then what will be the input current to get the result. And how?

n1ist
Support Volunteer
Posts: 1008
Joined: Wed Mar 22, 2006 11:02 am

Re: How to transfer power wirelessly by Infrared

Post by n1ist » Sat Jun 10, 2017 4:57 am

Once again, what exactly are you trying to do? You haven't mentioned how much power you are looking to transfer. Also, why are you modulating the light source? That just turns it off for part of the time, reducing available light.

Are you actually trying to transfer power, or are you making a beam-break or burglar alarm detector? If the latter, you can do it but will need optics and good alignment. For the former, you are probably looking at large optics, high powered lasers, or 1000W incandescent bulbs..

/mike

neverdie
Posts: 4
Joined: Thu Jul 13, 2017 10:52 am

Re: How to transfer power wirelessly by Infrared

Post by neverdie » Thu Jul 13, 2017 1:23 pm

Maybe try solar panels? Perhaps IR will excite them as much as visible light. Worth a try. You could use a columinator on your IR beam to help mitigate the square of the distance issue. Or preferably use an IR laser. As long as price and efficiency don't matter much, I'd say it's do-able.

Post Reply