Cannot Pair HC-08

All things pertaining to wireless and RF links

Moderator: phalanx

Post Reply
sanjay.thorat
Posts: 1
Joined: Thu Mar 23, 2017 12:50 am

Cannot Pair HC-08

Post by sanjay.thorat » Thu Mar 23, 2017 12:52 am

I have recently purchased a HC-08 Bluetooth module. When I connect to it via Arduino Mega, the blue light on it blinks and HC-08 device appears on my phone and computer while searching for bluetooth devices, but I am not able to pair with it. On PC, it says unable to pair and on phone it says password/pin is incorrect. When I send AT commands to the module, I do not get any response. Can you please help with this?

hc08nopair
Posts: 1
Joined: Fri Jun 02, 2017 5:14 am

Re: Cannot Pair HC-08

Post by hc08nopair » Fri Jun 02, 2017 5:27 am

I'm having the same problem. My setup is the same as yours, HC-08 on an arduino mega. It is attached to Serial1.

I did however get AT commands to work. With Serial <=> Serial1 passthrough:

AT
OK

AT+RX
Name:HC-08
Role:Slave
Baud:9600,NONE
Addr:50,65,83,9C,A4,52
PIN :000000

AT+VERSION
HC-08 V2.2,2015-07-30

So far I've tried to pair with it using three different android phones and a laptop, to no avail. I enabled experimental features (NOPLUGIN_OPTION="-E"), set the device as trusted, but whenever I try to connect it gives me "Failed to connect: org.bluez.Error.NotAvailable" and then after timeout "Failed to pair: org.bluez.Error.AuthenticationCanceled". Without setting trust, it gives "Failed to pair: org.bluez.Error.AuthenticationFailed" immediately.

brit_bodger
Posts: 1
Joined: Wed Aug 02, 2017 11:03 am

Re: Cannot Pair HC-08

Post by brit_bodger » Wed Aug 02, 2017 11:23 am

I have had the same problem, it's been driving me mad.
I'm using the Uno and have been able to use AT commands (@sanjay.thorat maybe try swooping the the RX and TX wires)

AT+RX

Name:HC-08
Role:Slave
Baud:9600,NONE
Addr:C8,FD,19,4E,67,2F
PIN :000000

AT+VERSION
HC-08 V2.2,2015-07-30

My HC 08 came part of a kit and the supplier has made an app that dose connect (so they clearly know something we don't). I have tried connecting it to my laptop and multiple other apps to no successes.
The app that came with it is called Elegoo BLE Tool if thats enough for you, but I want to use my laptop or an app with support for more pre-set buttons.

If anyone has found out a way round this please share. Thanks

jerxx94
Posts: 1
Joined: Thu Nov 16, 2017 4:34 pm

Re: Cannot Pair HC-08

Post by jerxx94 » Thu Nov 16, 2017 4:43 pm

Hi,

Upload this code and you'll be able to send AT commands.
void setup() {
// initialize both serial ports:
Serial.begin(9600);
Serial1.begin(9600);
}

void loop() {
// read from port 1, send to port 0:
if (Serial1.available()) {
int inByte = Serial1.read();
Serial.write(inByte);
}

// read from port 0, send to port 1:
if (Serial.available()) {
int inByte = Serial.read();
Serial1.write(inByte);

}
}
Then use the AT command AT+TYPE1 to be able to pair. Once you do that, use AT+PASS123456 to change the pairing pin to 123456. Then, you'll be able to pair using that pin.

Hope this helps

Post Reply