- Mon Jul 04, 2016 11:55 am
#190500
I'd like to use the XBee Shield with DIN and DOUT pins of XBee going to pins D12 and D13 on the Arduino.
I understand that I must "open" SJ1 and SJ3 solder jumpers.
After I have opened the jumpers, where on the XBee Shield can I pick up the OUT and IN signals? I can't cut the D2 and D3 pins as I need them for a shield higher in the stack. Note that IN and OUT are not directly connected to DIN and DOUT on the XBee.
Thanks for the help,
Chris Wood
I understand that I must "open" SJ1 and SJ3 solder jumpers.
After I have opened the jumpers, where on the XBee Shield can I pick up the OUT and IN signals? I can't cut the D2 and D3 pins as I need them for a shield higher in the stack. Note that IN and OUT are not directly connected to DIN and DOUT on the XBee.
Thanks for the help,
Chris Wood