- Sun Apr 24, 2016 1:09 pm
#189533
I'm using this library https://github.com/sparkfun/SparkFun_ES ... no_Library alongside a ESP8266 and Teensy. I'd like to make simple HTTP GET requests and print the plain text response to the serial monitor.
Below is the code I have so far. I've confirmed from my server's end that the request is coming through over the web. However, all I get in response from client.read() is '13'. You can see a sample of the actual server response at http://minitron.shivspatel.com/plain
Any ideas?
Below is the code I have so far. I've confirmed from my server's end that the request is coming through over the web. However, all I get in response from client.read() is '13'. You can see a sample of the actual server response at http://minitron.shivspatel.com/plain
Any ideas?
Code: Select all
#include <SoftwareSerial.h>
#include <SparkFunESP8266WiFi.h>
const char mySSID[] = "testnetwork";
const char myPSK[] = "password";
String server = "minitron.shivspatel.com";
String httpHeader = "GET /plain HTTP/1.1\r\nHost: minitron.shivspatel.com\r\nConnection: close\r\n\r\n";
void setup()
{
int status;
Serial.begin(9600);
status = esp8266.begin();
if (status <= 0)
{
Serial.println(F("Unable to communicate with shield. Looping"));
while(1) ;
}
esp8266.setMode(ESP8266_MODE_STA); // Set WiFi mode to station
if (esp8266.status() <= 0) // If we're not already connected
{
if (esp8266.connect(mySSID, myPSK) < 0)
{
Serial.println(F("Error connecting"));
while (1) ;
}
}
Serial.print(F("Station IP address: "));
Serial.println(esp8266.localIP());
Serial.println(F("Press any key to make a request..."));
}
void loop()
{
if (Serial.available())
{
httpGet();
while (Serial.available())
Serial.read();
}
}
void httpGet()
{
ESP8266Client client;
if (client.connect(server, 80) <= 0)
{
Serial.println(F("Failed to connect to minitron.shivspatel.com"));
return;
}
Serial.println(F("Making HTTP GET request to minitron.shivspatel.com"));
client.print(httpHeader);
Serial.println("Response:");
Serial.println(client.read());
if (client.connected())
client.stop();
}