We believe the Snapdragon IC contains additional frequency(s) and additional routines other than what Qualcomm has disclosed or is aware of for their integrated modem for the Snapdragon Processor SoC IC's. These additional frequency(s) are transmitting video data and transmitting and receiving special command data.
The entire video representation of the user's screen is being transmitted from the user's device by Snapdragon Processor (modem) IC and also this same IC is transmitting a specific unknown command at every break point as I call it or another words at every event driven interaction by the user. In the case of the transmission of a specific command the user's Snapdragon IC (modem) receives a return command from another similarly designed processor IC device which is in wireless range. For example a person is typing a note using a word editor on an Android smart phone then every key tap for a character will send out (transmit) a undisclosed command to another device nearby and the this other device sends back a "paste" command for example. so whatever is in the clipboard gets pasted right into the word editor. As long as the other nearby device sends a command which the word editor supports the command gets executed without any user intervention. A completely transparent process.
https://www.qualcomm.com/products/snapd ... essors/810