- Mon Feb 16, 2015 1:16 pm
#179780
I searching for a good/reliable RF CC2500 transmitter.
Can the Wixel be used to send data to a CC2500 client?
I’ve tried a Chinese CC2500 (actually a XL2500) as host but have trouble keeping steady communication.
It's a bit strange, it's not a range issue: it sometimes works 30 feet away and yet fails a few feet away and seems to be very location-dependent.
I know the CC2511 chip can do CC2500 communication but I’m not sure if the "Wixel" has been programmed with it’s own protocol so that it is not compatible with a generic CC2500.
I can't make changes to the client aside from what the sender can negotiate.
Some of the the CC2500 client params:
IF frequency of 253.9kHz
FREQ = 2420 MHz
CHANBW = 541.666 kHz
DRATE = 249.94 kBaud
MSK modulation, 30/32 sync word bits
FEC disabled,
2 preamble bytes
CHANSPC = 199.951 kHz
CHANNEL = 1
If the answer is yes, can the Wixel be outfitted with an external antenna to increase range?
Can the Wixel be used to send data to a CC2500 client?
I’ve tried a Chinese CC2500 (actually a XL2500) as host but have trouble keeping steady communication.
It's a bit strange, it's not a range issue: it sometimes works 30 feet away and yet fails a few feet away and seems to be very location-dependent.
I know the CC2511 chip can do CC2500 communication but I’m not sure if the "Wixel" has been programmed with it’s own protocol so that it is not compatible with a generic CC2500.
I can't make changes to the client aside from what the sender can negotiate.
Some of the the CC2500 client params:
IF frequency of 253.9kHz
FREQ = 2420 MHz
CHANBW = 541.666 kHz
DRATE = 249.94 kBaud
MSK modulation, 30/32 sync word bits
FEC disabled,
2 preamble bytes
CHANSPC = 199.951 kHz
CHANNEL = 1
If the answer is yes, can the Wixel be outfitted with an external antenna to increase range?