- Tue Jul 16, 2013 6:34 am
#161576
Hi,
I am trying to create TCP socket to connect to Wifly. I am trying to get connected via following code but its not working, no response from wifly. IP and port are correct and device is connected to adhoc wifi generated by wifly module. Let me know if I am doing any thing wrong.
I am trying to create TCP socket to connect to Wifly. I am trying to get connected via following code but its not working, no response from wifly. IP and port are correct and device is connected to adhoc wifi generated by wifly module. Let me know if I am doing any thing wrong.
Code: Select all
InetAddress serverAddr = InetAddress.getByName(SERVERIP);
Log.e("TCP Client", "C: Connecting...");
//create a socket to make the connection with the server
Socket socket = new Socket(serverAddr, SERVERPORT);
try {
//send the message to the server
out = new PrintWriter(new BufferedWriter(new OutputStreamWriter(socket.getOutputStream())), true);
Log.e("TCP Client", "C: Sent.");
Log.e("TCP Client", "C: Done.");
connected = true;
//receive the message which the server sends back
in = new BufferedReader(new InputStreamReader(socket.getInputStream()));
//in this while the client listens for the messages sent by the server
while (mRun) {
serverMessage = in.readLine();
if (serverMessage != null && mMessageListener != null) {
//call the method messageReceived from MyActivity class
mMessageListener.messageReceived(serverMessage);
}
serverMessage = null;
}
Log.e("RESPONSE FROM SERVER", "S: Received Message: '" + serverMessage + "'");
} catch (Exception e) {
Log.e("TCP", "S: Error", e);
} finally {
//the socket must be closed. It is not possible to reconnect to this socket
// after it is closed, which means a new socket instance has to be created.
socket.close();
}