Help with comment WiFly board to my WiFi network

All things pertaining to wireless and RF links

Moderator: phalanx

Post Reply
rgelb
Posts: 9
Joined: Tue Jan 18, 2011 1:17 am

Help with comment WiFly board to my WiFi network

Post by rgelb » Tue Jan 18, 2011 1:32 am

I am having trouble connecting the WiFly board to local WiFi network. I've tried it with security turned on (WPA2) and with it turned off, I keep getting Disconn from acumen4,AUTH-ERR. I am hoping someone can spot something. Here are results of a scan:

Code: Select all

SCAN:Found 1
Num            SSID   Ch  RSSI   Sec    MAC Address	Suites
 1              acumen4 09 -59    Open 00:0c:41:c2:56:c0   2104    0
Then I say: join acumen4. I get this in response:

Code: Select all

Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..
<2.20> 
Disconn from acumen4,AUTH-ERR
Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..

Disconn from acumen4,AUTH-ERR
Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..

Disconn from acumen4,AUTH-ERR
Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..

Associated!
DHCP: Start
So it seems like it worked, but it did not, because I send show net and get this in response (e.g. DHCP failed):

Code: Select all

SSid=acumen4
Chan=9
Assoc=OK
Rate=12, 24Mb
Auth=OK
Mode=OPEN
DHCP=FAIL
Boot=0
Time=OK
Links=1
<2.20>  
Here are the results of get everything for reference:

Code: Select all

WiFly Ver 2.20, 05-25-2010
Beacon=100
Probe=60
OPEN=*OPEN*
CLOSE=*CLOS*
REMOTE=*HELLO*
FlushSize=900
MatchChar=0
FlushTimer=10
IdleTimer=0
CmdChar=$
IF=DOWN
DHCP=ON
IP=0.0.0.0:2000
NM=0.0.0.0
GW=0.0.0.0
HOST=0.0.0.0:2000
PROTO=TCP,
MTU=1460
FLAGS=0x7
BACKUP=0.0.0.0
DNS=0.0.0.0
Name=server1
Backup=backup2
FTP=208.109.78.34:21
File=wifly-GSX.img
User=roving
Pass=Pass123
SSID=acumen4
Chan=0
ExtAnt=0
Join=1
Auth=OPEN
Mask=0x1fff
Rate=12, 24 Mb
Linkmon=0
Passphrase=rubygirl
SleepTmr=0
WakeTmr=0
Trigger=0x1
Autoconn=0
IoFunc=0x0
IoMask=0x20f0
PrintLvl=0x1
TimeEna=0
TIMEADR=129.6.15.28:123
Zone=7
Baudrate=115200
Flow=0x0
Mode=0x0
JoinTmr=1000
Replace=0x24
DeviceId=WiFly-GSX
Password=
Format=0x0
Sensors=0x0
BCAST=255.255.255.255:55555
Interval=0x7
<2.20> 
I've tried factory reset - did not work.
So what am I missing here?

follower
Posts: 280
Joined: Sun Mar 14, 2010 11:58 pm

Re: Help with comment WiFly board to my WiFi network

Post by follower » Tue Jan 18, 2011 3:24 pm

rgelb wrote:I am having trouble connecting the WiFly board to local WiFi network. I've tried it with security turned on (WPA2) and with it turned off, I keep getting Disconn from acumen4,AUTH-ERR. I am hoping someone can spot something. Here are results of a scan:

Code: Select all

SCAN:Found 1
Num            SSID   Ch  RSSI   Sec    MAC Address	Suites
 1              acumen4 09 -59    Open 00:0c:41:c2:56:c0   2104    0
The "Open" implies there is no password/phrase required.
Then I say: join acumen4. I get this in response:

Code: Select all

Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..
<2.20> 
Disconn from acumen4,AUTH-ERR
Is there MAC-based access control in use on your Access Point?

I would suggest looking at your Access Point logs for an error message.

Code: Select all

Disconn from acumen4,AUTH-ERR
Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..

Associated!
DHCP: Start
So it seems like it worked, but it did not, because I send show net and get this in response (e.g. DHCP failed):
Does your router list the WiFly module as successfully connected?

What model WiFi Access Point do you have?

--Philip;

rgelb
Posts: 9
Joined: Tue Jan 18, 2011 1:17 am

Re: Help with comment WiFly board to my WiFi network

Post by rgelb » Tue Jan 18, 2011 4:09 pm

The "Open" implies there is no password/phrase required.
Correct. As I mentioned I tried it with security and without. All the logs I posted were tried when I turned off security on the router.
Is there MAC-based access control in use on your Access Point?
No.
Does your router list the WiFly module as successfully connected?
I'll have a look at it tonight and will update the answer.
What model WiFi Access Point do you have?
Just your standard Linksys WG54 wireless router.

rgelb
Posts: 9
Joined: Tue Jan 18, 2011 1:17 am

Re: Help with comment WiFly board to my WiFi network

Post by rgelb » Tue Jan 18, 2011 11:25 pm

So I checked the router and, no, it does not show the WiFly module as being connected.
I also checked the router logs, but it only shows incoming and outgoing data requests, not connection requests, so nothing from the WiFly module.

One thing that I don't get is why I am getting an authorization error when trying to connect to a network with no security:

Code: Select all

Disconn from acumen4,AUTH-ERR
Another thing that is suspect to me (but keep in mind, i am a noob) are the following settings (when I hit get everything):

Code: Select all

User=roving
Pass=Pass123
Passphrase=rubygirl
Should I set these settings (i am assuming these are defaults) to empty, since the network is empty? If so, how do I set them to empty?

rgelb
Posts: 9
Joined: Tue Jan 18, 2011 1:17 am

Re: Help with comment WiFly board to my WiFi network

Post by rgelb » Wed Jan 19, 2011 12:37 am

Ok, the good news is that I got it working.

First, I happened upon a fella with a similar problem (viewtopic.php?f=13&t=24408), who suggested that bad grounding on the WiFly cards cause RF interference. So I moved the WiFly card as far away from the parent device as I could (few inches) and lo and behold it worked. It connected to a wifi network with NO security.

Then I tried to make it connect to a network with security and it just wouldn't do it. I kept on getting AUTH-ERR. I tried all types of supported security schemes (as listed in reference guide), but nothing worked. Finally, I nailed it down to my password having a space in it. The ref guide states that spaces should be replaced by $ dollar signs, but this does not work. When I changed the password not to contain spaces, everything worked great.

Hope this helps the next dude.

follower
Posts: 280
Joined: Sun Mar 14, 2010 11:58 pm

Re: Help with comment WiFly board to my WiFi network

Post by follower » Mon Feb 07, 2011 11:33 pm

Thanks for updating us with your solution.

--Philip;

strykeroz
Posts: 8
Joined: Sat Jan 07, 2012 5:19 am

Re: Help with comment WiFly board to my WiFi network

Post by strykeroz » Sat Jan 07, 2012 5:36 am

Hi

I'm getting the same symptoms as mentioned here, and in the original post regarding "bad grounding". Unfortunately I have a WiFly bee so moving it away from the Arduino isn't such an easy task. I'm also using a Bees shield, from Seeed, in case this detail matters.

I can connect to my notebook in adhoc mode, but no matter if I have security set or open on the my wlan the WiFly cycles through this behavior :

Code: Select all

Auto-Assoc CANEFIRE chan=11 mode=WEP SCAN OK
Joining CANEFIRE now..
Disconn from CANEFIRE,AUTH-ERR
Auto-Assoc CANEFIRE chan=11 mode=WEP SCAN OK
Joining CANEFIRE now..
Auto-Assoc CANEFIRE chan=11 mode=WEP SCAN OK
Joining CANEFIRE now..
Is there a way to improve the situation for a WiFly Bee by shielding it, or any other creative means? Happy to try whatever it takes.

Result of get everything :

Code: Select all

WiFly Ver 2.30, 10-26-2011 on RN-171
Beacon=100
Probe=5
Reboot=0
OPEN=*OPEN*
CLOSE=*CLOS*
REMOTE=
FlushSize=75
MatchChar=9
FlushTimer=2000
IdleTimer=30
CmdChar=$
IF=DOWN
DHCP=OFF
IP=192.168.34.166:80
NM=255.255.255.0
GW=192.168.34.1
HOST=0.0.0.0:2000
PROTO=TCP,
MTU=1524
FLAGS=0x7
TCPMODE=0x0
BACKUP=0.0.0.0
DNS=161.72.0.0
Name=server1
Backup=backup2
FTP=208.109.78.34:21
File=wifly-EZX.img
User=roving
Pass=Pass123
Dir=public
Timeout=40
FTP_mode=0x0
SSID=CANEFIRE
Chan=0
ExtAnt=0
Join=1
Auth=WEP
Mask=0x1fff
Rate=12, 24 Mb
Linkmon=5
Keynum=1
Key=b2 d4 f6 8b af bd c3 d3 d4 ec 5b 48 64
TxPower=0
SleepTmr=0
WakeTmr=0
Trigger=0x1
Autoconn=1
IoFunc=0x0
IoMask=0x21f0
IoValu=0x0
DebugReg=0x0
PrintLvl=0x1
TimeEna=15
TIMEADR=255.255.255.255:123
Zone=7
Baudrate=9600
Flow=0x0
Mode=0x1
JoinTmr=1000
Replace=0x24
DeviceId=WiFly-EZX
Password=
Format=0x0
Signal=0
Average=5
BCAST=255.255.255.255:55555
Interval=0x7
Sensor=0x0
SensePwr=0x0
The Netgear APs on the home wlan will only bridge & repeat using WEP in case you're wondering why I'm bothering with that. They're due to be replaced in a month or so, but can bring that forward too in the unlikely event that's contributing to this issue.

Thanks for any advice you can offer,
Geoff

strykeroz
Posts: 8
Joined: Sat Jan 07, 2012 5:19 am

Re: Help with comment WiFly board to my WiFi network

Post by strykeroz » Thu Jan 19, 2012 5:07 am

FYI replacing the Netgear 11G AP's which were running WEP with a new 11N setup running WPA2 has resolved this issue.

Post Reply