- Sun Jul 25, 2010 3:52 pm
#106014
Hi, I know this is a popular topic . So I've been using two pairs of 434MHz TX and RX modules (WRL-08946 and WRL-08949) without any issues (I run them at 1200baud since that is more reliable and gets better distance). I've used the KLP Sparkfun tutorial and have moved on to using a small RFDriver library and it works great, I get reliable data transmitted across the link with zero noise.
So I ordered two sets of 315MHz modules (two TX/WRL-08945 and two RX/WRL-08947) a while back from Sparkfun thinking it would be an easy way to have another transmitter operate in the same vicinity without interference. I just tried them out in my circuit and I'm not receiving anything. The 315's and 434's are pin-compatible and I just swapped the boards on both sides (TX & RX), receiving side no longer gets data. Using a radio scanner I can clearly hear the transmitter signal at about 315MHz, but I'm not getting data into my Arduino on the receiving side. Connecting an oscilloscope up to the data output line on the receiver board proves that it's only outputting a flatline 5V, no data. Normally you get noise when there is no signal, but I'm not even getting that. Tried both sets of 315MHz boards, same thing with either set. I've tried running them at 4800, 2400, 1200, and 300 baud to no affect. The last thing I just tried was increasing voltage to the 315MHz TX from 5v to 9v thinking that perhaps these boards just require a stronger signal to get anything across. This has not changed anything, although my scanner can pick up the 315MHz TX further away at 9V.
Again, the 434's work fine in the exact same circuit, the evidence seems to lean towards both the 315MHz RX boards being toast. Anyone have something else I can try? Maby there's something I've still missed in this process.
Thanks!
So I ordered two sets of 315MHz modules (two TX/WRL-08945 and two RX/WRL-08947) a while back from Sparkfun thinking it would be an easy way to have another transmitter operate in the same vicinity without interference. I just tried them out in my circuit and I'm not receiving anything. The 315's and 434's are pin-compatible and I just swapped the boards on both sides (TX & RX), receiving side no longer gets data. Using a radio scanner I can clearly hear the transmitter signal at about 315MHz, but I'm not getting data into my Arduino on the receiving side. Connecting an oscilloscope up to the data output line on the receiver board proves that it's only outputting a flatline 5V, no data. Normally you get noise when there is no signal, but I'm not even getting that. Tried both sets of 315MHz boards, same thing with either set. I've tried running them at 4800, 2400, 1200, and 300 baud to no affect. The last thing I just tried was increasing voltage to the 315MHz TX from 5v to 9v thinking that perhaps these boards just require a stronger signal to get anything across. This has not changed anything, although my scanner can pick up the 315MHz TX further away at 9V.
Again, the 434's work fine in the exact same circuit, the evidence seems to lean towards both the 315MHz RX boards being toast. Anyone have something else I can try? Maby there's something I've still missed in this process.
Thanks!