When I use this code:
I get this error
"The Client has been renamed as EthernetClient"
Console:
Code: Select allsketch_apr30a.ino:3:2: error: #endif without #if
sketch_apr30a:22: error: no matching function for call to 'Client::Client(byte [4], int)'
As of Arduino 1.0, the Client class in the Ethernet library has been renamed to EthernetClient.
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:7: note: candidates are: Client::Client()
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:7: note: Client::Client(const Client&)
sketch_apr30a:22: error: cannot declare variable 'client' to be of abstract type 'Client'
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:7: note: because the following virtual functions are pure within 'Client':
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:12: note: virtual size_t Client::write(uint8_t)
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:13: note: virtual size_t Client::write(const uint8_t*, size_t)
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:14: note: virtual int Client::available()
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:15: note: virtual int Client::read()
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:17: note: virtual int Client::peek()
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:18: note: virtual void Client::flush()
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:10: note: virtual int Client::connect(IPAddress, uint16_t)
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:11: note: virtual int Client::connect(const char*, uint16_t)
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:16: note: virtual int Client::read(uint8_t*, size_t)
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:19: note: virtual void Client::stop()
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:20: note: virtual uint8_t Client::connected()
C:\Program Files (x86)\Arduino\hardware\arduino\cores\arduino/Client.h:21: note: virtual Client::operator bool()
sketch_apr30a.ino: In function 'void loop()':
sketch_apr30a:53: error: expected `)' before '{' token
I am using a WiFly shield not an EthernetShield, how do I fix This problem?
I hope someone could help me as soon as possible

thanks