- Wed Nov 26, 2008 8:42 pm
#60075
I recently bought two nrf2401a modules <http://www.sparkfun.com/commerce/produc ... cts_id=152> along with the accompanying development nodes <http://www.sparkfun.com/commerce/produc ... cts_id=713> -utilizing the infamous PIC 16F88- from Spark Fun.
I was able to successfully compile (version V01*** of the code provided by SFE using CC5X) and program the modules using WinPic and the PG1 programmer from Olimex/SFE. My problem is that I am not sure whether the transceivers are communicating. I have a couple of questions that I DESPERATELY need help with:
1) How do you modify the code [notably version 1 from SFE] so as to see the data transferred to either of the modules. I was going to rely on the LED’s on the development nodes but one of them on ONE of the board seems to have taken an early thanksgiving break!....
I've tried using a rs232 data logger from Eltima Software but unfortunately I only able to get a text file filled with white spaces.
2) Also, in the manual Nordic manual the transceiver seems to require 143 bits for configuration but the code seems to only mention 24 bits (0-23) seen below:
config_setup[0] = 0b.0000.0101;
config_setup[1] = 0b.0100.1110;
config_setup [2] = 0b.0010.0011;
***Here’s the code I am trying to implement on the transceivers:
/*
nRF2401 test code to run on the 24G demo board, V01
This code will generate AUTOMATICALLY send and recieve packets from another demo board running the same V01 code.
This code does not accept user input.
Compiles with the free version of CC5X
Pete Dokter, 2/22/06
config_setup word 16 bits found on pages 13-15
23: 0 Payloads have an 8 bit address
22: 0
21: 1
20: 0
19: 0
18: 0
17: 1 16-Bit CRC
16: 1 CRC Enabled
15: 0 One channel receive
14: 1 ShockBurst Mode
13: 0 250K Transmission Rate
12: 0
11: 1
10: 1
9: 1 RF Output Power
8: 0 RF Output Power
7: 0 Channel select (channel 2)
6: 0
5: 0
4: 0
3: 0
2: 1
1: 0
0: 0 Transmit mode
*/
#define Clock_8MHz
#define Baud_9600
#include "C:\Global\PIC\C\16F88.h"
#pragma config |= 0x3F30 //Internal Oscillator, No WDT, MCLR Enabled
//#include "C:\Global\PIC\C\Stdio.c" // Basic Serial IO
#define CS PORTA.0 //out
#define CLK1 PORTA.1 //out
#define DATA1 PORTA.2 //I/O
#define DR1 PORTA.3 //in
#define DATA2 PORTA.4 //in
#define CE PORTA.6 //out
#define CLK2 PORTA.7 //out
#define DR2 PORTB.0 //in
#define stat1 PORTB.1 //out
#define stat2 PORTB.3 //out
#define stat3 PORTB.4 //out
uns8 data_array[4];
//uns8 counter;
void boot_up(void);
void configure_receiver(void);
void configure_transmitter(void);
void transmit_data(void);
void receive_data(void);
void delay_ms(uns16);
void main()
{
uns8 x;
boot_up();
for (x = 0; x < 3; x++)
{
stat1 = 1;
delay_ms(25);
stat1 = 0;
stat2 = 1;
delay_ms(25);
stat2 = 0;
stat3 = 1;
delay_ms(25);
stat3 = 0;
}
stat1 = 1;
while(1)
{
configure_transmitter();
transmit_data();
configure_receiver();
delay_ms(50);
if(DR1 == 1) //We have data!
{
receive_data();
if ((data_array[0] == 0x12) && (data_array[1] == 0x34) && (data_array[2] == 0xAB) && (data_array[3] == 0xCD))
{
if (stat3 == 1)
{
stat3 = 0;
stat1 = 1;
}
else if (stat2 == 1)
{
stat2 = 0;
stat3 = 1;
}
else if (stat1 == 1)
{
stat1 = 0;
stat2 = 1;
}
}
}
}
}
void boot_up(void)
{
OSCCON = 0b.0111.0000; //Setup internal oscillator for 8MHz
while(OSCCON.2 == 0); //Wait for frequency to stabilize
ANSEL = 0b.0000.0000; //Turn pins to Digital instead of Analog
CMCON = 0b.0000.0111; //Turn off comparator on RA port
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1100; //0 = Output, 1 = Input
PORTB = 0b.0000.0000;
TRISB = 0b.1100.0101; //0 = Output, 1 = Input
//enable_uart_TX(0);
//enable_uart_RX(0);
}
//This will clock out the current payload into the data_array
void receive_data(void)
{
uns8 i, j, temp;
CE = 0;//Power down RF Front end
//Erase the current data array so that we know we are looking at actual received data
data_array[0] = 0x00;
data_array[1] = 0x00;
data_array[2] = 0x00;
data_array[3] = 0x00;
//Clock in data, we are setup for 32-bit payloads
for(i = 0 ; i < 4 ; i++) //4 bytes
{
for(j = 0 ; j < 8 ; j++) //8 bits each
{
temp <<= 1;
temp.0 = DATA1;
CLK1 = 1;
CLK1 = 0;
}
data_array = temp; //Store this byte
}
//if(RX_DR == 0) //Once the data is clocked completely, the receiver should make DR go low
//printf("DR went low\n\r", 0);
//printf("\n\rData Received:\n\r", 0);
//printf("[0] : %h\n\r", data_array[0]);
//printf("[1] : %h\n\r", data_array[1]);
//printf("[2] : %h\n\r", data_array[2]);
//printf("[3] : %h\n\r", data_array[3]);
CE = 1; //Power up RF Front end
}
//This sends out the data stored in the data_array
//data_array must be setup before calling this function
void transmit_data(void)
{
uns8 i, j, temp, rf_address;
data_array[0] = 0x12;
data_array[1] = 0x34;
data_array[2] = 0xAB;
data_array[3] = 0xCD;
CE = 1;
delay_ms(1);
//Clock in address
rf_address = 0b.1110.0111; //Power-on Default for all units (on page 11)
for(i = 0 ; i < 8 ; i++)
{
DATA1 = rf_address.7;
CLK1 = 1;
CLK1 = 0;
rf_address <<= 1;
}
//Clock in the data_array
for(i = 0 ; i < 4 ; i++) //4 bytes
{
temp = data_array;
for(j = 0 ; j < 8 ; j++) //One bit at a time
{
DATA1 = temp.7;
CLK1 = 1;
CLK1 = 0;
temp <<= 1;
}
}
CE = 0; //Start transmission
}
//2.4G Configuration - Receiver
//This setups up a RF-24G for receiving at 1mbps
void configure_receiver(void)
{
uns8 i,j;
//uns24 config_setup;
uns8 config_setup[3], temp;
//During configuration of the receiver, we need DATA1 as an output
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1000; //0 = Output, 1 = Input (DR1 is on RA3) (DATA1 is on RA2)
//Config Mode
CE = 0; CS = 1;
delay_ms(1);
//Setup configuration word, set up for 250k
//config_setup = 0b.0010.0011.0100.1110.0000.0101; //Look at pages 13-15 for more bit info
config_setup[0] = 0b.0000.0101;
config_setup[1] = 0b.0100.1110;
config_setup[2] = 0b.0010.0011;
/*//purchased version
for(i = 0 ; i < 24 ; i++)
{
DATA1 = config_setup.23;
CLK1 = 1;
CLK1 = 0;
config_setup <<= 1;
}
*/
//free version
for (j = 3; j > 0; j--)
{
for(i = 0 ; i < 8 ; i++)
{
DATA1 = config_setup[j-1].7;
CLK1 = 1;
CLK1 = 0;
config_setup[j-1] <<= 1;
}
}
//Configuration is actived on falling edge of CS (page 10)
CE = 0; CS = 0;
//After configuration of the receiver, we need DATA1 as an input
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1100; //0 = Output, 1 = Input (DR1 is on RA3) (DATA1 is on RA2)
delay_ms(1);
//Start monitoring the air
CE = 1; CS = 0;
//printf("RX Configuration finished...\n\r", 0);
}
//2.4G Configuration - Transmitter
//This sets up one RF-24G for shockburst transmission
void configure_transmitter(void)
{
uns8 i,j;
//uns24 config_setup;
uns8 config_setup[3], temp;
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1000; //0 = Output, 1 = Input (DR1 is on RA3) (DATA1 is on RA2)
//Config Mode
CE = 0; CS = 1;
delay_ms(1);
//Delay of 5us from CS to Data (page 30) is taken care of by the for loop
//Setup configuration word
//config_setup = 0b.0010.0011.0100.1110.0000.0100; //Look at pages 13-15 for more bit info
config_setup[0] = 0b.0000.0100;
config_setup[1] = 0b.0100.1110;
config_setup[2] = 0b.0010.0011;
/*//purchased version
for(i = 0 ; i < 24 ; i++)
{
DATA1 = config_setup.23;
CLK1 = 1;
CLK1 = 0;
config_setup <<= 1;
}
*/
//free version
for (j = 3; j > 0; j--)
{
for(i = 0 ; i < 8 ; i++)
{
DATA1 = config_setup[j-1].7;
CLK1 = 1;
CLK1 = 0;
config_setup[j-1] <<= 1;
}
}
delay_ms(1);
//Configuration is actived on falling edge of CS (page 10)
CE = 0; CS = 0;
//printf("TX Configuration finished...\n\r", 0);
}
//General short delay
void delay_ms(uns16 x)
{
uns8 y, z;
for ( ; x > 0 ; x--)
for ( y = 0 ; y < 4 ; y++)
for ( z = 0 ; z < 176 ; z++);
}
I was able to successfully compile (version V01*** of the code provided by SFE using CC5X) and program the modules using WinPic and the PG1 programmer from Olimex/SFE. My problem is that I am not sure whether the transceivers are communicating. I have a couple of questions that I DESPERATELY need help with:
1) How do you modify the code [notably version 1 from SFE] so as to see the data transferred to either of the modules. I was going to rely on the LED’s on the development nodes but one of them on ONE of the board seems to have taken an early thanksgiving break!....
I've tried using a rs232 data logger from Eltima Software but unfortunately I only able to get a text file filled with white spaces.
2) Also, in the manual Nordic manual the transceiver seems to require 143 bits for configuration but the code seems to only mention 24 bits (0-23) seen below:
config_setup[0] = 0b.0000.0101;
config_setup[1] = 0b.0100.1110;
config_setup [2] = 0b.0010.0011;
***Here’s the code I am trying to implement on the transceivers:
/*
nRF2401 test code to run on the 24G demo board, V01
This code will generate AUTOMATICALLY send and recieve packets from another demo board running the same V01 code.
This code does not accept user input.
Compiles with the free version of CC5X
Pete Dokter, 2/22/06
config_setup word 16 bits found on pages 13-15
23: 0 Payloads have an 8 bit address
22: 0
21: 1
20: 0
19: 0
18: 0
17: 1 16-Bit CRC
16: 1 CRC Enabled
15: 0 One channel receive
14: 1 ShockBurst Mode
13: 0 250K Transmission Rate
12: 0
11: 1
10: 1
9: 1 RF Output Power
8: 0 RF Output Power
7: 0 Channel select (channel 2)
6: 0
5: 0
4: 0
3: 0
2: 1
1: 0
0: 0 Transmit mode
*/
#define Clock_8MHz
#define Baud_9600
#include "C:\Global\PIC\C\16F88.h"
#pragma config |= 0x3F30 //Internal Oscillator, No WDT, MCLR Enabled
//#include "C:\Global\PIC\C\Stdio.c" // Basic Serial IO
#define CS PORTA.0 //out
#define CLK1 PORTA.1 //out
#define DATA1 PORTA.2 //I/O
#define DR1 PORTA.3 //in
#define DATA2 PORTA.4 //in
#define CE PORTA.6 //out
#define CLK2 PORTA.7 //out
#define DR2 PORTB.0 //in
#define stat1 PORTB.1 //out
#define stat2 PORTB.3 //out
#define stat3 PORTB.4 //out
uns8 data_array[4];
//uns8 counter;
void boot_up(void);
void configure_receiver(void);
void configure_transmitter(void);
void transmit_data(void);
void receive_data(void);
void delay_ms(uns16);
void main()
{
uns8 x;
boot_up();
for (x = 0; x < 3; x++)
{
stat1 = 1;
delay_ms(25);
stat1 = 0;
stat2 = 1;
delay_ms(25);
stat2 = 0;
stat3 = 1;
delay_ms(25);
stat3 = 0;
}
stat1 = 1;
while(1)
{
configure_transmitter();
transmit_data();
configure_receiver();
delay_ms(50);
if(DR1 == 1) //We have data!
{
receive_data();
if ((data_array[0] == 0x12) && (data_array[1] == 0x34) && (data_array[2] == 0xAB) && (data_array[3] == 0xCD))
{
if (stat3 == 1)
{
stat3 = 0;
stat1 = 1;
}
else if (stat2 == 1)
{
stat2 = 0;
stat3 = 1;
}
else if (stat1 == 1)
{
stat1 = 0;
stat2 = 1;
}
}
}
}
}
void boot_up(void)
{
OSCCON = 0b.0111.0000; //Setup internal oscillator for 8MHz
while(OSCCON.2 == 0); //Wait for frequency to stabilize
ANSEL = 0b.0000.0000; //Turn pins to Digital instead of Analog
CMCON = 0b.0000.0111; //Turn off comparator on RA port
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1100; //0 = Output, 1 = Input
PORTB = 0b.0000.0000;
TRISB = 0b.1100.0101; //0 = Output, 1 = Input
//enable_uart_TX(0);
//enable_uart_RX(0);
}
//This will clock out the current payload into the data_array
void receive_data(void)
{
uns8 i, j, temp;
CE = 0;//Power down RF Front end
//Erase the current data array so that we know we are looking at actual received data
data_array[0] = 0x00;
data_array[1] = 0x00;
data_array[2] = 0x00;
data_array[3] = 0x00;
//Clock in data, we are setup for 32-bit payloads
for(i = 0 ; i < 4 ; i++) //4 bytes
{
for(j = 0 ; j < 8 ; j++) //8 bits each
{
temp <<= 1;
temp.0 = DATA1;
CLK1 = 1;
CLK1 = 0;
}
data_array = temp; //Store this byte
}
//if(RX_DR == 0) //Once the data is clocked completely, the receiver should make DR go low
//printf("DR went low\n\r", 0);
//printf("\n\rData Received:\n\r", 0);
//printf("[0] : %h\n\r", data_array[0]);
//printf("[1] : %h\n\r", data_array[1]);
//printf("[2] : %h\n\r", data_array[2]);
//printf("[3] : %h\n\r", data_array[3]);
CE = 1; //Power up RF Front end
}
//This sends out the data stored in the data_array
//data_array must be setup before calling this function
void transmit_data(void)
{
uns8 i, j, temp, rf_address;
data_array[0] = 0x12;
data_array[1] = 0x34;
data_array[2] = 0xAB;
data_array[3] = 0xCD;
CE = 1;
delay_ms(1);
//Clock in address
rf_address = 0b.1110.0111; //Power-on Default for all units (on page 11)
for(i = 0 ; i < 8 ; i++)
{
DATA1 = rf_address.7;
CLK1 = 1;
CLK1 = 0;
rf_address <<= 1;
}
//Clock in the data_array
for(i = 0 ; i < 4 ; i++) //4 bytes
{
temp = data_array;
for(j = 0 ; j < 8 ; j++) //One bit at a time
{
DATA1 = temp.7;
CLK1 = 1;
CLK1 = 0;
temp <<= 1;
}
}
CE = 0; //Start transmission
}
//2.4G Configuration - Receiver
//This setups up a RF-24G for receiving at 1mbps
void configure_receiver(void)
{
uns8 i,j;
//uns24 config_setup;
uns8 config_setup[3], temp;
//During configuration of the receiver, we need DATA1 as an output
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1000; //0 = Output, 1 = Input (DR1 is on RA3) (DATA1 is on RA2)
//Config Mode
CE = 0; CS = 1;
delay_ms(1);
//Setup configuration word, set up for 250k
//config_setup = 0b.0010.0011.0100.1110.0000.0101; //Look at pages 13-15 for more bit info
config_setup[0] = 0b.0000.0101;
config_setup[1] = 0b.0100.1110;
config_setup[2] = 0b.0010.0011;
/*//purchased version
for(i = 0 ; i < 24 ; i++)
{
DATA1 = config_setup.23;
CLK1 = 1;
CLK1 = 0;
config_setup <<= 1;
}
*/
//free version
for (j = 3; j > 0; j--)
{
for(i = 0 ; i < 8 ; i++)
{
DATA1 = config_setup[j-1].7;
CLK1 = 1;
CLK1 = 0;
config_setup[j-1] <<= 1;
}
}
//Configuration is actived on falling edge of CS (page 10)
CE = 0; CS = 0;
//After configuration of the receiver, we need DATA1 as an input
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1100; //0 = Output, 1 = Input (DR1 is on RA3) (DATA1 is on RA2)
delay_ms(1);
//Start monitoring the air
CE = 1; CS = 0;
//printf("RX Configuration finished...\n\r", 0);
}
//2.4G Configuration - Transmitter
//This sets up one RF-24G for shockburst transmission
void configure_transmitter(void)
{
uns8 i,j;
//uns24 config_setup;
uns8 config_setup[3], temp;
PORTA = 0b.0000.0000;
TRISA = 0b.0011.1000; //0 = Output, 1 = Input (DR1 is on RA3) (DATA1 is on RA2)
//Config Mode
CE = 0; CS = 1;
delay_ms(1);
//Delay of 5us from CS to Data (page 30) is taken care of by the for loop
//Setup configuration word
//config_setup = 0b.0010.0011.0100.1110.0000.0100; //Look at pages 13-15 for more bit info
config_setup[0] = 0b.0000.0100;
config_setup[1] = 0b.0100.1110;
config_setup[2] = 0b.0010.0011;
/*//purchased version
for(i = 0 ; i < 24 ; i++)
{
DATA1 = config_setup.23;
CLK1 = 1;
CLK1 = 0;
config_setup <<= 1;
}
*/
//free version
for (j = 3; j > 0; j--)
{
for(i = 0 ; i < 8 ; i++)
{
DATA1 = config_setup[j-1].7;
CLK1 = 1;
CLK1 = 0;
config_setup[j-1] <<= 1;
}
}
delay_ms(1);
//Configuration is actived on falling edge of CS (page 10)
CE = 0; CS = 0;
//printf("TX Configuration finished...\n\r", 0);
}
//General short delay
void delay_ms(uns16 x)
{
uns8 y, z;
for ( ; x > 0 ; x--)
for ( y = 0 ; y < 4 ; y++)
for ( z = 0 ; z < 176 ; z++);
}