- Tue May 06, 2008 4:56 pm
#47748
I purchased a Bluetooth Modem - BlueSMiRF Silver and having connection issues. Hope someone can help. I am using on a PC/xpsp2 native drivers. First I must say I have one of their older models and it worked from the get-go!
The BlueSMiRF Silver communicates from a Pic 16f88 (as did the other one that works) but all I get is garbage out this new one. So that sounds like the baud rate or other setting are not the same as the PC. One problem is that I can't figure out how to get into the command mode. I have tried all different combination. Reading the doc. it says to use the escape char. which is +++ as the default. I get no response from it. I'm using HyperTerminal on the PC. I have tried all the possible baud rates on the PC but no luck. If I could figure out how to get into the command mode I could set the baud rate on the device or at least see what it is. Anybody have an ideas where to go from here?
The BlueSMiRF Silver communicates from a Pic 16f88 (as did the other one that works) but all I get is garbage out this new one. So that sounds like the baud rate or other setting are not the same as the PC. One problem is that I can't figure out how to get into the command mode. I have tried all different combination. Reading the doc. it says to use the escape char. which is +++ as the default. I get no response from it. I'm using HyperTerminal on the PC. I have tried all the possible baud rates on the PC but no luck. If I could figure out how to get into the command mode I could set the baud rate on the device or at least see what it is. Anybody have an ideas where to go from here?