M6e Nano issue with URA

All things pertaining to wireless and RF links

Moderator: phalanx

Post Reply
Tash777
Posts: 3
Joined: Tue May 23, 2017 4:06 am

M6e Nano issue with URA

Post by Tash777 » Tue May 23, 2017 4:19 am

Hi everybody,

I am just wondering if anybody else is having an issue when using the universal reader assistant with the SparkFun Simultaneous RFID Reader - M6E Nano

Using the SparkFun Serial Basic Breakout - CH340G, It will connect and I can set all the settings, antenna power below 5dbm as I am using the USB as a power supply. When I hit the read tags it reads for about 4 seconds and then comes up with an error

- Connection to the reader is lost. Disconnect the reader.

I do have log files if anybody can help or is there something silly that I am missing?


Thanks in advance.

JHus
Posts: 1
Joined: Thu Aug 03, 2017 8:14 am

Re: M6e Nano issue with URA

Post by JHus » Thu Aug 03, 2017 8:18 am

Hi, I have the same problem.

For me however, the single read option kinda works (a few times, then it says it has no more acces to the com port).
The continuous read option doesnt work at all. The reading light turns green, but a second or so later, you can hear the windows sound telling you that the usb device is disconnecting. Software hangs and have to reconnect etc.

Tried to set the read power below 5 but still doesn't work.

Anyone knows what the problem could be?

cheers

piezoplaty
Posts: 2
Joined: Sat Oct 14, 2017 9:44 pm

Re: M6e Nano issue with URA

Post by piezoplaty » Sat Oct 14, 2017 9:47 pm

I too am having trouble with the Universal Reader Assistant. I get reads for ~10 seconds, then the disconnect occurs.

piezoplaty
Posts: 2
Joined: Sat Oct 14, 2017 9:44 pm

Re: M6e Nano issue with URA

Post by piezoplaty » Sat Oct 28, 2017 1:20 pm

I connected an external power supply to the M6e, and it seems have resolved the issue.

My setup originally used an external antenna drawing power from USB. No matter how low I set the read power, the thing would only run for ~10 seconds.

With the external power, I'm able to run 27dBm without issue.

paulvha
Posts: 207
Joined: Sat Nov 11, 2017 2:39 am

Re: M6e Nano issue with URA

Post by paulvha » Sat Nov 11, 2017 2:47 am

An external power supply should be applied to use full antenna power. Depending on your USB it might deliver enough for other antenna power (USB 2.0 is standard for 500mA, 3.0 for 800mA). Otherwise the module will random loose connection.

rubikadams
Posts: 1
Joined: Thu Feb 22, 2018 10:28 pm

Re: M6e Nano issue with URA

Post by rubikadams » Thu Feb 22, 2018 10:40 pm

I don´t have lecture at all using the URA, I been instaled the " 64-bit installer for Universal Reader Assistant 3.4 from API 1.29.4" on my windows 10 ¿some one at Spark fun can help us? please

paulvha
Posts: 207
Joined: Sat Nov 11, 2017 2:39 am

Re: M6e Nano issue with URA

Post by paulvha » Fri Feb 23, 2018 6:32 am

works perfect for me.. what com port are you connecting to ? what kind of issues to you experience ?

Post Reply