12C Bootloader

Support for Bloader and Screamer

Moderator: phalanx

Post Reply
MrPotatoHead
Posts: 72
Joined: Thu Mar 20, 2008 9:55 am

12C Bootloader

Post by MrPotatoHead » Mon Oct 18, 2010 2:54 pm

Hi,

I am using a PIC18F25K22 in my current project (8 Channel 1A LED Driver). The unit will be a I2C slave. I would like to use the I2C for a bootloader.

In the final system version, there will be two circuit types. The LED driver I2C slave. There may be multiple iterations of it on the bus. The second circuit is the I2C master. It will have the option to connect to a PC via USB. I would like to use the master board to reprogram the slave boards via USB and the I2C.

Any recommendations? Thanks in advance.

- joseph Y.

Post Reply