HID Bootloader + MPLAB SIM

Support for Bloader and Screamer

Moderator: phalanx

HID Bootloader + MPLAB SIM

Postby wscrosswy » Thu Jul 22, 2010 11:38 am

Hey all,

I'm having issues running my modified Microchip Applications Library USB Joystick demo in MPLAB SIM. The project compiles and works fine on the PIC itself, but not in MPLAB SIM. I try to run the program and it starts at the top of Boot Flash memory and gives 200

"CORE-W0018: Instruction at 0x... decoded as Reserved (NOP)"

errors before execution halts. I'm wondering if it has to do with the fact that the program is designed to be used with the HID bootloader. Thoughts?

Posts: 13
Joined: Sun Feb 07, 2010 10:51 pm

Re: HID Bootloader + MPLAB SIM

Postby EmbeddedMan » Tue Aug 03, 2010 9:46 pm

Yup, I'm sure that's what your problem is. Re-compile without support for the bootloader and it should work fine.

User avatar
Support Volunteer
Posts: 1362
Joined: Sun Mar 05, 2006 9:23 pm

Return to Boot Loading

Who is online

Users browsing this forum: No registered users and 2 guests