Thank you for your response. I'll try to address the issues you bring up here.
About the 6 Volt issue - I was replying to Ghazans message - if you follow the conversation:
- Ghazan Wrote:
...I also tried a 6.5V wallwart for a short while, the issue did not disappear.
- rstickley wrote:
...If you supply 6 volts to the board, you are supplying 6 volts to the USB port.
- Olimex wrote:
...you should not apply 6V, there is PTC fuses on the USB host port for overcurrent protection but none for overvoltage protection
Notice that this little tidbit of information is not noted anywhere in any Olimex documentation. In fact, this is overlooked by the distributor
as Sparkfun sells this board with a "related" item:
$3.00 Wall Adapter Power Supply - 6VDC 300mA
http://www.sparkfun.com/commerce/produc ... ts_id=8208
For future reference, you should note this in your documentation (and maybe let your distributors know also) but thanks for the confirmation.
- Olimex wrote:
welcome to the embedded world
Thank you - after 23 years of embedded development I now feel welcomed!:)
But, lets remember, this started as an ethernet issue (see topic title)
- Olimex wrote:
....Something should be worng with your cables
- Olimex wrote:
...should provide 5V 1A power supply.
What you left off is the exact part number of the supply that works with this board. I have 5 wall warts from 5 different manufactures which output 5V or more at 1 Amp or more. All 5 exhibit exactly the same response on the Ethernet port.
OK, maybe these are not "top quality" wall warts, but they are probably typical of the output you can expect from wall warts in general.
Notice, what was not said:
- Nobody wrote:
...we will try several different supplies and see what happens.
Also, we got no response to the "short C84" work around - maybe you should explain why this works (if you understood that, then you would understand why our supplies do not work either).
- rstickley wrote:
According to the Micrel KS8721BL/SL datasheet - Feb. 2005, the:
"MDIO Pull-up resistor value changed to 4.7k?."
Is this a problem ? Is there any reason you are not following the datasheet ? Does your board stop being "flakey" if you fix this error on your board?
Why is there no response to either of these issues?
- Olimex wrote:
"how many ARM9 boards you have been used so far"
Three different arm boards - two with Cirrus ARM processors and an Atmel ARM eval board.
I'm just getting started but these all seem to work.
- Olimex wrote:
"I don't know what are your support expectations"
Maybe respond to our questions.
Maybe provide more than one sheet of documentation?
Maybe explain why we are having these problems ?
- Olimex wrote:
All boards we ship are subjet to multiply tests
Sounds great - do you test the USB port? and the SD Card Port ?
please post your test so we can see how to setup and test these ports on our boards...
- Olimex wrote:
Regarding your "hardware" issue, let me know how to track problem which doesn't exist when we test the boards at our place?
Listen and learn. Listen to the posts on this forum. Duplicate the problem at your factory, analyze the hardware and learn why this problem exists in the first place.
- Olimex wrote:
"if you have good power supply with 5V 1A you will never have problems"
Please define a "good power supply" - manufacturer and part number.
Thanks for your help,
Ralph