Logomatic Low freq?

Everything ARM and LPC

Moderator: phalanx

Post Reply
Chris-toph
Posts: 2
Joined: Sun Jan 03, 2016 7:58 am

Logomatic Low freq?

Post by Chris-toph » Sun Jan 03, 2016 8:25 am

Is there an expert could explain and let me know the exact settings I should apply to monitor at low frequency (in the range of 1 measurement/per hour) with the logomatic (data logger)?
If I understood correctly with T0MR0, which is a 32 bit variable, I can set to the maximum of 2^32 = 4294967296 -> 4294967296 / 58982400 = 72 s.
Is there a way to get a slower frequency rate?
As I'm a novice, I would appreciate if you could let me know how the exact changes I have to do in the code of the main.c file?
Many thanks for your help.
Christoph

Chris-toph
Posts: 2
Joined: Sun Jan 03, 2016 7:58 am

Re: Logomatic Low freq?

Post by Chris-toph » Sat Jan 09, 2016 6:09 pm

In case you want to operate the logomatic at down to 1 per min (0.01667 Hz), I'v modified the main.c file accordingly.
Set for instance in the logcon.txt file "Frequency = .01667". Max 6 digits.
Attachments
FW.SFE.txt
(37.59 KiB) Downloaded 51 times
main.c
(24.84 KiB) Downloaded 50 times

Post Reply