SparkFun Forums 

Where electronics enthusiasts find answers.

Everything ARM and LPC
By Chris-toph
#187003
Is there an expert could explain and let me know the exact settings I should apply to monitor at low frequency (in the range of 1 measurement/per hour) with the logomatic (data logger)?
If I understood correctly with T0MR0, which is a 32 bit variable, I can set to the maximum of 2^32 = 4294967296 -> 4294967296 / 58982400 = 72 s.
Is there a way to get a slower frequency rate?
As I'm a novice, I would appreciate if you could let me know how the exact changes I have to do in the code of the main.c file?
Many thanks for your help.
Christoph
By Chris-toph
#187198
In case you want to operate the logomatic at down to 1 per min (0.01667 Hz), I'v modified the main.c file accordingly.
Set for instance in the logcon.txt file "Frequency = .01667". Max 6 digits.
You do not have the required permissions to view the files attached to this post.