Setup:
Windows 8.1
Eclipse Luna
Most recent WinARM
LPC11U68 Demo board from NXP
So I downloaded eclipse, installed CDT, and connected it with the GCC Arm compiler. I have eclipse compiling code and I think its working. It produces a list file that makes sense to me as its primarily just loads and stores needed anyways. My code is very simple, I just turn off PIO2_18 as can be seen in the code below. I have an LED connected to power and then back to the pin. A low signal would then illuminate the LED.
Code: Select all
#define GPIO_ADDR_PIO2_18 0x4004413C
#define DIR2 (((volatile unsigned int *) (0xA0002008)))
#define PORT2 (((volatile unsigned int *)(0xA0002108)))
int main (void) {
//setup pin functions
*GPIO2_18 = 0x0000;
//setup pin direction
*DIR2 = (1 << 18);
*PORT2 = (1 << 18);
//disable clock to conserve power
while (1) /* Loop forever */
{
*PORT2 = (0 << 18);
}
}
The only output from eclipse that I can get are a .elf and a .hex file. I need a .bin as the LPC11U68 appears as a thumb drive to load code. In order to do this I am using arm-elf-objdump. I dont remember the exact command off the top of my head though. This produces a .bin file that I than copy and paste into the LPC board. When I reset/apply power it jumps right back into the bootloader as if my code was never even installed.
Anybody have any experience with this? Are there any specific toolchain settings I need to know of?
One thought that I had was the format of the ELF file. Is there any ELF parser out there that can read the elf file and give me a view of what it has?
Another thought is that there is actually more initialization needed. Is this so?
I just need a push in the right direction...