- Wed Dec 31, 2014 5:47 am
#178199
Hi everyone! 
I try to receive data from UDA1380 chip(ADC/DAC) by I2S. Could you tell me if my config is ok? I still get interrrupt and only 000000.. appear in UART terminal

I try to receive data from UDA1380 chip(ADC/DAC) by I2S. Could you tell me if my config is ok? I still get interrrupt and only 000000.. appear in UART terminal

Code: Select all
I hope you can help because nobody could. Thanks in advance!/*
===============================================================================
Name : kodek.c
Author : $(author)
Version :
Copyright : $(copyright)
Description : main definition
===============================================================================
*/
#ifdef __USE_CMSIS
#include "LPC407x_8x.h"
#endif
#include "lpc_i2s.h"
#include "lpc_pinsel.h"
#include "uda1380.h"
#include "debug_frmwrk.h"
int main(void) {
debug_frmwrk_init();
int8_t ret;
I2S_MODEConf_Type I2S_ClkConfig;
I2S_CFG_Type I2S_ConfigStruct;
volatile uint32_t i;
PINSEL_ConfigPin(0,7,1); //TX
PINSEL_ConfigPin(0,8,1);
PINSEL_ConfigPin(0,9,1);
PINSEL_ConfigPin(0,23,2); //RX
PINSEL_ConfigPin(0,24,2);
PINSEL_ConfigPin(0,25,2);
PINSEL_ConfigPin(1,16,2); //MCLK
I2S_Init(LPC_I2S);
/* Audio Config*/
I2S_ConfigStruct.wordwidth = I2S_WORDWIDTH_16;
I2S_ConfigStruct.mono = I2S_STEREO;
I2S_ConfigStruct.stop = I2S_STOP_DISABLE;
I2S_ConfigStruct.reset = I2S_RESET_ENABLE;
I2S_ConfigStruct.ws_sel = I2S_MASTER_MODE;
I2S_ConfigStruct.mute = I2S_MUTE_DISABLE;
I2S_Config(LPC_I2S,I2S_TX_MODE,&I2S_ConfigStruct);
I2S_ConfigStruct.ws_sel = I2S_SLAVE_MODE;
I2S_Config(LPC_I2S,I2S_RX_MODE,&I2S_ConfigStruct);
/* Clock Mode Config*/
I2S_ClkConfig.clksel = I2S_CLKSEL_MCLK;
I2S_ClkConfig.fpin = I2S_4PIN_DISABLE;
I2S_ClkConfig.mcena = I2S_MCLK_ENABLE;
I2S_ModeConfig(LPC_I2S,&I2S_ClkConfig,I2S_TX_MODE);
I2S_ModeConfig(LPC_I2S,&I2S_ClkConfig,I2S_RX_MODE);
I2S_FreqConfig(LPC_I2S, 44100, I2S_TX_MODE);
I2S_SetBitRate(LPC_I2S,0,I2S_RX_MODE);
//I2S_Stop(LPC_I2S, I2S_TX_MODE);
I2S_Stop(LPC_I2S, I2S_RX_MODE);
I2S_IRQConfig(LPC_I2S,I2S_TX_MODE,4);
I2S_IRQCmd(LPC_I2S,I2S_RX_MODE,ENABLE);//przerwanie przy odbiorze
LPC_I2S->RXBITRATE = 0;
LPC_I2S->RXRATE = 0;
for(i = 0; i <0x1000000; i++); // delay
ret = Uda1380_Init(200000, 32000);
if(ret==0){
DEBUGOUT("Inicjalizacja kodek OK \r\n");
}else{
_DBD(ret);
}
for(i = 0; i <0x3000000; i++); // delay
I2S_Start(LPC_I2S);
NVIC_EnableIRQ(I2S_IRQn);
while(1){
}
return 0;
}
void I2S_IRQHandler()
{
uint32_t input = LPC_I2S->RXFIFO;
_DBD32(input);
DEBUGOUT("\r\n");
}