Ugh, I confess I'm not sure if I love Eclipse or hate it. Sorry about the delayed response. At least you have the command line tools working.
I have experience only with LPC and STM32 parts - it is possible there is something odd about SAM7 that is tripping you up.
I just installed the current version of Eclipse (4.3.1) on Fedora 20. After considerable floundering I got a simple STM32F4Discovery project up. It gave a choice of standard (CDI) debugger framework or GDB (DSF). I chose standard since that has worked in the past. With verbose console checked I got the following dump. Mostly gibberish to me, but
seems clear enough.
Code: Select allgdb-set confirm off
256^done
(gdb)
257-gdb-set width 0
257^done
(gdb)
258-gdb-set height 0
258^done
(gdb)
259-interpreter-exec console echo
259^done
(gdb)
260-gdb-show prompt
260^done,value="(gdb) "
(gdb)
261-gdb-set new-console on
261^error,msg="No symbol table is loaded. Use the \"file\" command."
(gdb)
262 symbol-file /media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build/stm.o
&"symbol-file /media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build/stm.o\n"
symbol-file /media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build/stm.o
262^done
(gdb)
263-target-select remote localhost:3333
=thread-group-started,id="i1",pid="42000"
=thread-created,id="1",group-id="i1"
*stopped,frame={addr="0x080002e8",func="Reset_Handler",args=[]},thread-id="1",stopped-threads="all"
263^connected
(gdb)
264 load /media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build/stm.o
&"load /media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build/stm.o \n"
~"Loading section .isr_vector, size 0x188 lma 0x8000000\n"
264+download,{section=".isr_vector",section-size="392",total-size="3421"}
~"Loading section .text, size 0x1b0 lma 0x8000188\n"
264+download,{section=".text",section-size="432",total-size="3421"}
~"Start address 0x8000188, load size 824\n"
~"Transfer rate: 1 KB/sec, 412 bytes/write.\n"
264^done
(gdb)
265 info proc
&"info proc\n"
&"Undefined info command: \"proc\". Try \"help info\".\n"
265^error,msg="Undefined info command: \"proc\". Try \"help info\"."
266 info program
(gdb)
&"info program\n"
~"Debugging a target over a serial line.\n"
~"Program stopped at 0x80002e8.\n"
~"It stopped with signal SIGINT, Interrupt.\n"
~"Type \"info stack\" or \"info registers\" for more information.\n"
266^done
267 info threads
(gdb)
&"info threads\n"
~" Id Target Id Frame \n"
~"* 1 Remote target 0x08000188 in ?? ()\n"
267^done
268-stack-info-depth
(gdb)
268^done,depth="3"
269-stack-list-frames 0 3
(gdb)
269^done,stack=[frame={level="0",addr="0x08000188",func="??"},frame={level="1",addr="0xfffffffe",func="??"},frame={level="2",addr="0xfffffffe",func="??"}]
270-data-list-changed-registers
(gdb)
270^done,changed-registers=["0","1","2","3","4","5","6","7","8","9","10","11","12","13","14","15","16","17","18","19","20","21","22","23","24","25"]
271 info sharedlibrary
(gdb)
&"info sharedlibrary\n"
~"No shared libraries loaded at this time.\n"
271^done
(gdb)
272-environment-directory /media/slug1/code/arm/stm32f4discovery/gpio/gpiod /media/slug1/code/chiplib/st/Libraries/CMSIS/Include /media/slug1/code/chiplib/st/Libraries/CMSIS/Device/ST/STM32F4xx/Include /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4 /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv6-m /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv6-m/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/fpu /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/fpu/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/softfp /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/softfp/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-m /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-m/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/fpu /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/fpu/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/softfp /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/softfp/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/fpu /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/fpu/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/thumb /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/thumb/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/backward /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/bits /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/debug /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/decimal /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/bin_search_tree_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/binary_heap_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/binomial_heap_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/binomial_heap_base_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/branch_policy /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/cc_hash_table_map_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/eq_fn /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/gp_hash_table_map_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/hash_fn /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/left_child_next_sibling_heap_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/list_update_map_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/list_update_policy /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/ov_tree_map_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/pairing_heap_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/pat_trie_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/rb_tree_map_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/rc_binomial_heap_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/resize_policy /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/splay_tree_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/thin_heap_ /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/tree_policy /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/trie_policy /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/unordered_iterator /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/profile /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/profile/impl /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/tr1 /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/tr2 /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/machine /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/rpc /home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/sys /media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build /media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build/obj /media/slug1/code/chiplib/st/Libraries/CMSIS/Device/ST/STM32F4xx/Source/Templates/gcc_ride7
272^done,source-path="/media/slug1/code/arm/stm32f4discovery/gpio/gpiod:/media/slug1/code/chiplib/st/Libraries/CMSIS/Include:/media/slug1/code/chiplib/st/Libraries/CMSIS/Device/ST/STM32F4xx/Include:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv6-m:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv6-m/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/fpu:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/fpu/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/softfp:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-ar/thumb/softfp/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-m:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7-m/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/fpu:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/fpu/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/softfp:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/armv7e-m/softfp/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/fpu:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/fpu/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/thumb:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/arm-none-eabi/thumb/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/backward:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/bits:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/debug:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/decimal:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/bin_search_tree_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/binary_heap_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/binomial_heap_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/binomial_heap_base_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/branch_policy:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/cc_hash_table_map_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/eq_fn:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/gp_hash_table_map_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/hash_fn:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/left_child_next_sibling_heap_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/list_update_map_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/list_update_policy:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/ov_tree_map_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/pairing_heap_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/pat_trie_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/rb_tree_map_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/rc_binomial_heap_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/resize_policy:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/splay_tree_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/thin_heap_:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/tree_policy:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/trie_policy:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/ext/pb_ds/detail/unordered_iterator:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/profile:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/profile/impl:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/tr1:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/c++/4.7.4/tr2:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/machine:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/rpc:/home/hfs2/toolchain/linaro/2013q3/arm-none-eabi/include/sys:/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build:/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/build/obj:/media/slug1/code/chiplib/st/Libraries/CMSIS/Device/ST/STM32F4xx/Source/Templates/gcc_ride7:$cdir:$cwd"
273-data-list-register-names
(gdb)
273^done,register-names=["r0","r1","r2","r3","r4","r5","r6","r7","r8","r9","r10","r11","r12","sp","lr","pc","f0","f1","f2","f3","f4","f5","f6","f7","fps","cpsr","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","","",""]
(gdb)
274-break-insert main.c:9
274^done,bkpt={number="1",type="breakpoint",disp="keep",enabled="y",addr="0x080001c6",func="main",file="main.c",fullname="/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/main.c",line="9",times="0",original-location="main.c:9"}
(gdb)
275-break-insert main.c:11
275^done,bkpt={number="2",type="breakpoint",disp="keep",enabled="y",addr="0x080001d4",func="main",file="main.c",fullname="/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/main.c",line="11",times="0",original-location="main.c:11"}
(gdb)
276-break-insert main.c:12
276^done,bkpt={number="3",type="breakpoint",disp="keep",enabled="y",addr="0x080001ec",func="main",file="main.c",fullname="/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/main.c",line="12",times="0",original-location="main.c:12"}
(gdb)
277-stack-list-arguments 0 0 0
277^done,stack-args=[frame={level="0",args=[]}]
(gdb)
278-stack-list-locals 0
278^done,locals=[]
(gdb)
279-exec-continue
~"Note: automatically using hardware breakpoints for read-only addresses.\n"
Note: automatically using hardware breakpoints for read-only addresses.
279^running
*running,thread-id="all"
(gdb)
=breakpoint-modified,bkpt={number="1",type="breakpoint",disp="keep",enabled="y",addr="0x080001c6",func="main",file="main.c",fullname="/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/main.c",line="9",times="1",original-location="main.c:9"}
*stopped,reason="breakpoint-hit",disp="keep",bkptno="1",frame={addr="0x080001c6",func="main",args=[],file="main.c",fullname="/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/main.c",line="9"},thread-id="1",stopped-threads="all"
(gdb)
280 info threads
&"info threads\n"
~" Id Target Id Frame \n"
~"* 1 Remote target main () at main.c:9\n"
280^done
(gdb)
281-stack-info-depth
281^done,depth="1"
(gdb)
282-stack-list-frames 0 1
282^done,stack=[frame={level="0",addr="0x080001c6",func="main",file="main.c",fullname="/media/slug1/code/arm/stm32f4discovery/gpio/gpiod/main.c",line="9"}]
283-data-list-changed-registers
(gdb)
283^done,changed-registers=["2","3","7","13","15"]
284 info sharedlibrary
(gdb)
&"info sharedlibrary\n"
~"No shared libraries loaded at this time.\n"
284^done
(gdb)
285-stack-list-arguments 0 0 0
285^done,stack-args=[frame={level="0",args=[]}]
(gdb)
286-stack-list-locals 0
286^done,locals=[]
(gdb)
Not sure what to check next. I could attempt to set up with Yagarto, but if the issue is SAM7 specific that won't help. I'd be happy to post some screen shots.